Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Cirrus Logic Audio Card on RPI 2 with Windows 10
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 2 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 618 views
  • Users 0 members are here
  • raspberry_pi
Related

Cirrus Logic Audio Card on RPI 2 with Windows 10

tamirkrispis
tamirkrispis over 10 years ago

Hi,

 

I want to develop some audio applications using my Raspberry Pi 2 running windows 10 on it, I need to be able to both record and play high quality audio (minimum 16 bit / 44.1 Khz).

 

Would the Cirrus Logic Audio Card do the trick? Can it work with Win 10?

 

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    tamirkrispis

         The Raspberry Pi 2 can use the Cirrus Logic Audio Card using Linux img with correct drivers. It can alsu run as Windows 10 IOT connected to a Windows 10 PC which is a requirement to load application code. But it cannot run both because Windows 10 IOT does not have Cirrus drivers (yet?). You may have to pester Cirrus logic to write drivers, but that is unlikely since 99% that use the card prefer Linux instead of Windows 10 IOT. What I would do is choose what you need most for the project. If you give more details, I may be able to get more speific here.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tamirkrispis
    0 tamirkrispis over 10 years ago in reply to clem57

    Hi Clem,

    First I would like to thank you for your reply.

     

    I would like to record audio using a RPI2 and save it to the SD card on the RPI2 as an audio file, the audio source is an analog audio feed coming from an outside source such as a musical instrument or mp3 player (Does the card has a line in?). I also want to be able to play the recorded and stored audio files from the SD card back to the user.

     

    I would like the audio to be with good quality, at least as CD quality (16bit/44.1khz).

     

    I wanted to go Windows IOT as I'm more familiar with that environment and the C# programming language.

    But, I would be glad to hear your suggestion on using the right OS and development language, are you suggesting using the Respbian (or other flavor of Linux) with Python, C or Java as a programming language? which would be best for my requirements while using the cirrus logic audio card?

     

    Thanks!

    clem57

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tamirkrispis
    0 tamirkrispis over 10 years ago in reply to clem57

    Hi Clem,

    First I would like to thank you for your reply.

     

    I would like to record audio using a RPI2 and save it to the SD card on the RPI2 as an audio file, the audio source is an analog audio feed coming from an outside source such as a musical instrument or mp3 player (Does the card has a line in?). I also want to be able to play the recorded and stored audio files from the SD card back to the user.

     

    I would like the audio to be with good quality, at least as CD quality (16bit/44.1khz).

     

    I wanted to go Windows IOT as I'm more familiar with that environment and the C# programming language.

    But, I would be glad to hear your suggestion on using the right OS and development language, are you suggesting using the Respbian (or other flavor of Linux) with Python, C or Java as a programming language? which would be best for my requirements while using the cirrus logic audio card?

     

    Thanks!

    clem57