Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using the raspberry Pi 2 mod B to programming arduino with a usb externally powered hub
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Subscribers 709 subscribers
  • Views 3716 views
  • Users 0 members are here
  • arduino uno
  • raspberry-pi2
  • com_port
  • usb 2.0 hub
Related

Using the raspberry Pi 2 mod B to programming arduino with a usb externally powered hub

e14 Contributor
e14 Contributor over 10 years ago

HI i have started to use a usb externally powered hub due to power demands of arduino and current drops in rpi but when i connect the usb cable from hub to arduino port is not available in ide. I dont understand i mean i tried various things like

> i am in dialout group

> latest usb drivers usbutils

> i checked the lsusb hub seems to work fine

> ohh and one thing i noticed usb keyboard or mouse or anyother HID device wont work with rpi when pluged into USB hub but storage devices like external HDD and flash drives work with hub // hub is fine tho i checked it on other system it works fine.

> my config : rpi 2 mod b+ 1GB( 2.1 A power supply)  /  OS debian (arm kali linux)  / 2 HID's 1 USB hub (connected)

i dont understand how do i make it work?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Start with R Pi powered from wall not usb hub. Also Arduino powered on jack from wall not usb hub. If this works, then the current/voltage on the hub is too low to handle the load. Many powered hubs are not up to the job.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    Start with R Pi powered from wall not usb hub. Also Arduino powered on jack from wall not usb hub. If this works, then the current/voltage on the hub is too low to handle the load. Many powered hubs are not up to the job.

    Clem