Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using the raspberry Pi 2 mod B to programming arduino with a usb externally powered hub
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 25 replies
  • Subscribers 709 subscribers
  • Views 3674 views
  • Users 0 members are here
  • arduino uno
  • raspberry-pi2
  • com_port
  • usb 2.0 hub
Related

Using the raspberry Pi 2 mod B to programming arduino with a usb externally powered hub

e14 Contributor
e14 Contributor over 10 years ago

HI i have started to use a usb externally powered hub due to power demands of arduino and current drops in rpi but when i connect the usb cable from hub to arduino port is not available in ide. I dont understand i mean i tried various things like

> i am in dialout group

> latest usb drivers usbutils

> i checked the lsusb hub seems to work fine

> ohh and one thing i noticed usb keyboard or mouse or anyother HID device wont work with rpi when pluged into USB hub but storage devices like external HDD and flash drives work with hub // hub is fine tho i checked it on other system it works fine.

> my config : rpi 2 mod b+ 1GB( 2.1 A power supply)  /  OS debian (arm kali linux)  / 2 HID's 1 USB hub (connected)

i dont understand how do i make it work?

  • Sign in to reply
  • Cancel
Parents
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    To AS:

    Pls post what you did/going-to-do WRT the powering your Arduino Uno R3. Did/does the Arduino Documentation have something more specific than (possibly) Cutting pin 1 of the Full Size Female type -B Connector w/ signal designation "+" (5v)? AAR I do not have a Arduino Uno R3. I do have a Arduino Variant, an Inland-brand Mega 2560 r3. This has less documentation than Real Arduinos.

    BTW (I have a 26pin GPIO RaspPi) to able to measure the Current requirements of your Arduino Uno R3, try buying a 40pin Pirack. My (26pin) Pirack Board has (jumpers) that you can bridge w/ an Ahm-Meter. IDK the p/n for the 40pin version, BUT the 26pin version IS; Manf: PiFace Newark P/n 97W2503 Manf p/n Pirack

    BTW2

    [Time Stamp 29FEB16 10:11AM EST] They just announced a RaspPi 3. This is a Game-Changer, b/c this RaspPi 3 has BT (BlueTooth). If a new (incarnation) of RaspPi Zero has

    BT, Then ALL BETS ARE OFF! The lack of wireless connectivity had forced us to use Microcontrollers. Not anymore, if a new RaspPi Zero includes BT. Any new RaspPi Zero including BT coupled w/ a RTC module for RaspPi (connected via GPIO Pins), will be a Great Combo. So await/Lobby-for a RaspPi Zero w/ BT

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    To AS:

    Pls post what you did/going-to-do WRT the powering your Arduino Uno R3. Did/does the Arduino Documentation have something more specific than (possibly) Cutting pin 1 of the Full Size Female type -B Connector w/ signal designation "+" (5v)? AAR I do not have a Arduino Uno R3. I do have a Arduino Variant, an Inland-brand Mega 2560 r3. This has less documentation than Real Arduinos.

    BTW (I have a 26pin GPIO RaspPi) to able to measure the Current requirements of your Arduino Uno R3, try buying a 40pin Pirack. My (26pin) Pirack Board has (jumpers) that you can bridge w/ an Ahm-Meter. IDK the p/n for the 40pin version, BUT the 26pin version IS; Manf: PiFace Newark P/n 97W2503 Manf p/n Pirack

    BTW2

    [Time Stamp 29FEB16 10:11AM EST] They just announced a RaspPi 3. This is a Game-Changer, b/c this RaspPi 3 has BT (BlueTooth). If a new (incarnation) of RaspPi Zero has

    BT, Then ALL BETS ARE OFF! The lack of wireless connectivity had forced us to use Microcontrollers. Not anymore, if a new RaspPi Zero includes BT. Any new RaspPi Zero including BT coupled w/ a RTC module for RaspPi (connected via GPIO Pins), will be a Great Combo. So await/Lobby-for a RaspPi Zero w/ BT