Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum PiFace Digital 2 - Free GPIO pins?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 2127 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

PiFace Digital 2 - Free GPIO pins?

Matt
Matt over 10 years ago

Is there a list of which GPIO pins are unused when you've got a PiFace Digital 2 attached to a Raspberry Pi 2. I'd like to solder on a 1-wire DS18B20 temperature sensor.

 

Thanks in advance,

 

Matt.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Seems like SPI is used mostly with a few pins as chip select(?). I would steal the I2C pins and use as digital since they would most logical be not used. Let me know if this works.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Matt
    0 Matt over 10 years ago in reply to clem57

    Thanks Clem. Chris Stanton mentioned that I should try to trace the lines on the board to the pins.. and doing that shows that the board only uses 3 pins (excl. 5v).. it should mean I can take my pick of the GPIO headers for my central heating home automation project image

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Matt
    0 Matt over 10 years ago in reply to Matt

    On further inspection.. SCLK is also wired up.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dan-cristian
    0 dan-cristian over 7 years ago in reply to Matt

    GPIO 25 pin is also wired and needed for input event listener.

    I noticed the board also needs 3.3 Volts power pins connected, even when is powered with an external source. Without 3.3 V power the board is sometimes not detected (random behaviour).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dan-cristian
    0 dan-cristian over 7 years ago in reply to Matt

    GPIO 25 pin is also wired and needed for input event listener.

    I noticed the board also needs 3.3 Volts power pins connected, even when is powered with an external source. Without 3.3 V power the board is sometimes not detected (random behaviour).