Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 3 und EnOcean Pi - Kompatibilitätsproblem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 49 replies
  • Answers 10 answers
  • Subscribers 711 subscribers
  • Views 7772 views
  • Users 0 members are here
  • raspberry-pi3
  • raspberry_pi_space
  • enoceanpi
Related

Raspberry Pi 3 und EnOcean Pi - Kompatibilitätsproblem

robertheinze
robertheinze over 10 years ago

Als diese Woche der neue RPi3 rauskam, waren wir voller Ehrgeiz, künftig in unseren Systemen zu switchen.

Immerhin würde der RPi3 es ermöglichen auf einen USB Bluetooth Dongle zu verzichten und eine WiFi-Connectivity macht die Verbindung zu unseren Servern noch einfacher .

 

leider weit gefeht, denn das ganze funkt nur unter Verwendung der SDIOs und UART (durch Aktivierung der Devce Tree-Funktionwn, was dann jedoch den EnOceanPi, der ebenfalls /dev/ttyAMA0 (UART) verwendet, außer Betrieb setzt. Sprich, wir haben es noch nicht geschafft, EnOceanPi, WiFi und Bluetooth am RPi3 zum Laufen zu bringen.

 

Hat wer, der mehr Erfahrung mit HW-orientierter Programmierung hat eine Idee?

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    0 cstanton over 10 years ago

    So you're saying that the WiFi/Bluetooth on the Pi3 uses the same ttyAMA0 UART as the Enocean Pi?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robertheinze
    0 robertheinze over 10 years ago in reply to cstanton

    Yes, thats exactly the situation

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 10 years ago in reply to robertheinze

    It appears the problem is that the baud rate of the UART is tied to the core clock speed:

     

    Es scheint, das Problem ist, dass die Baudrate des UART mit dem Kerntaktfrequenz gebunden ist:

     

    https://www.raspberrypi.org/forums/viewtopic.php?f=63&t=138162

     

    Also here in discussion:

     

    Raspberry Pi 3 Model B GPIO 40 Pin Block Pinout

     

    Also raised on github:

     

    https://github.com/RPi-Distro/repo/issues/22

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • robertheinze
    0 robertheinze over 10 years ago in reply to cstanton

    But when I disable the device tree, the EnOceanPi works perfectly. But WiFi and BT don't

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 10 years ago in reply to robertheinze

    Because when you're disabling the device tree you're disabling all of the configuration settings that make the Pi 3 work  with the GPIO mappings to be setup as they should be.

     

    As usual make sure your Raspbian is up to date with apt-get and firmware with rpi-update.

     

    Not using the device tree will change more settings than just that of the UART mapping.

     

    So it looks like this may be fixed in the next firmware update for the pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • cstanton
    0 cstanton over 10 years ago in reply to robertheinze

    Because when you're disabling the device tree you're disabling all of the configuration settings that make the Pi 3 work  with the GPIO mappings to be setup as they should be.

     

    As usual make sure your Raspbian is up to date with apt-get and firmware with rpi-update.

     

    Not using the device tree will change more settings than just that of the UART mapping.

     

    So it looks like this may be fixed in the next firmware update for the pi.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • robertheinze
    0 robertheinze over 10 years ago in reply to cstanton

    I will give it a try tomorrow , keep you updated ...

    thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to robertheinze

    Solution maybe this

    It is related. ttyAMA0 on a Pi3 is configured to communicate with the Bluetooth modem. 

     

    Disable just blue-tooth in DT fixes this and allows your situation.

    Clem