I want to use Rasbery Pi for lecture capture. Please advise how to do it.
I want to use Rasbery Pi for lecture capture. Please advise how to do it.
Is this in central location? It only has one channel for one camera/audio. If does not include the camera or microphone.
clem
Wow. Then expect the budget to increase by an order of magnitude, $200-$300k would not be unreasonable!
Alternatively, you could train the teachers to present using a PC, and then use something like webex..
I have not purchased it as yet. Am just surfing around. But if I get all the video and the audio to a central location, then for every classroom, I would need to have a recording system. Avermedia makes a better product. http://gamerzone.avermedia.com/game_capture/extremecap_u3
The teachers could be trained to use laptops for presentation but all may not agree to. Further, this process takes time.
You've described a couple of different scenarios. In the video, they showed the setup that Clem initially proposed. A raspberry pi, with a camera in a microphone in a room. That is pretty easy to setup.
You then added the complexity of sending that video/audio data to a central location to be controlled by an operator. Clem pointed out the the Pi probably doesn't have the IO bandwidth for that.
It would be inexpensive to setup 1 pi per room, then transfer the recorded video after the fact via network.
You could easily mimic the setup they show in the video, and compromise on the central control and data capture.
Mike
So there's your answer(!).
If you think that solution is available for download or purchase, why not obtain or purchase it?
Otherwise, you'd have to either design a solution using the Pi, or expect to pay what an off-the-shelf solution costs.
I like this suggestion. However, the classrooms continue for 4 hours and I wonder how long a footage can be captured by the raspberry PI. Secondly, how do I get the Pi to start and stop recording. I guess I could feed the rasperry PI and audio feed from my mixer to enable high quality audio being recorded too. I am open to all options.
You could even run a web server on the Pi and have the lecturer start the recording via smartphone or PC. Or it could be started remotely by the operator in a remote location, but they might need a cue to be gin recording, you might be able to stream the audio to the operator, or put a keyframe on the web site to cue them when to start the recording.
Mike
I think I've answered a couple of the questions. Duration of recording will be determined by the quality of the recording. 64gb and 128gb sd cards are available.
http://studiopost.com/contact/tech-specs/calculating-disk-space-requirements
That is a link to storage requirements for recording hd video.
You might have to compromise on the quality, but if this is for web quality viewing it may be doable.
Mike