I want to use Rasbery Pi for lecture capture. Please advise how to do it.
I want to use Rasbery Pi for lecture capture. Please advise how to do it.
What is the recording capacity of the PI ?
It's only limited to the size of the attached storage. As I said you can get very large SD cards, or hook a drive up via usb. But that might limit your usb bandwidth if that is also the source of your camera, but if you went with the pi camera you would have no such limit, and the external storage could be a multi terabyte drive.
Mike
How far from the PI can the storage device be kept while being connected by a USB cable?
Yes, this is for the central location. It does not include the camera and the mic or the PA system. All that would have to be procured and paid for but the quality could be much better.
Thank you. Now to revise everything, I need to purchase the raspberry PI and its camera and a USB flash drive. Then I would need to feed the Raspberry PI with an audio feed from the audio mixer that is in every classroom and then I have everything I need. Am I right?
I am unable to understand how the recording will be started, paused and stopped though. How will the raspberry get the command? Our teachers do not carry with them laptops.
A smartphone could work, or as I said you could add a little web program that would allow a remote operator to start the recording, but they would need to know when. Also, you could add a simple circuit with a button and a resistor to start the recording, there are really a number of possibilities, read up a little bit while you are waiting for you RasPi's, etc to show up. If you have questions, open a new thread and ask for help. There are a lot of people here that are willing to help if you are willing to gain a little knowledge to ask the right questions.
I'd advise you to start small, prototype the process and components, then replicate when you think you have a system in place that is satisfactory.
Good luck on this,
Mike
BTW, the circuitry and programming required to do this isn't real difficult. Anyone with a desire to learn can have this going pretty quickly.
Mike
Naresh,
"I'd advise you to start small, prototype the process and components, then replicate when you think you have a system in place that is satisfactory."
What Michael says here is so important!
You need to consider taking your time in finding the right solution to your needs. Prototype it, try various alternatives. Personally, i would not use HD video, but if the text that is written on the blackboard needs to be legible in the video then you might not have any other choice. For four hours of HD video you are looking at 6GB minimum, and I am just guessing. This page might help:
http://studiopost.com/contact/tech-specs/calculating-disk-space-requirements
Test at various definitions, use the minimum that meets your needs. Test it by watching a test video (needs to be 4 hours) to determine how usable it will be.
Good luck! Sgarciav
Where can I purchase the raspberry PI and the case and the camera?