Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi Zero Ethernet Problem
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 32 replies
  • Answers 5 answers
  • Subscribers 709 subscribers
  • Views 7624 views
  • Users 0 members are here
  • ethernet
  • raspberry pi
Related

Raspberry Pi Zero Ethernet Problem

e14 Contributor
e14 Contributor over 10 years ago

I'm having trouble connecting my Raspberry Pi zero to ethernet.

 

I have a Raspberry Pi 3 and four Raspberry Pi zeros. I'm a grad student in mathematics and I do a whole lot of parallel computing. I'm trying to set these up as a cluster to test my distributed code before I send it up to the university's very expensive computing cluster. I bought a handful of uxcell ethernet to micro USB adapters that you can find here: Amazon.com: uxcell Micro USB to RJ45 Network Card Adapter Converter for Windows 98SE Me: Computers & Accessories

 

When I plug ethernet into the Pi zero using this cable, the Pi zero is not being assigned an IP address. Is this adapter incorrect? I was hoping to use these cheap adapters as the grad student stipend isn't exactly CEO pay image.  As an additional note, plugging the ethernet directly into the Pi 3 works fine. The Pi 3 instantly recognizes the ethernet and has no problem connecting to the network.

 

I have tried using ip link and dhcpcd to get the network going on the Pi Zeros, but i'm stuck as I can't get them to recognize the LAN. I'm also positive that it isn't an issue with the router as I have used multiple routers (at home and at the university) and neither has worked. Thank you in advance for your replies.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Just a quick check is the otg  plugged to a powered hub with enough current? Mine was not because I needed more than 100 mA which was not provided as my picture setup showed.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Actually I am having a lot of trouble with my USB hub, and I'll be purchasing another one. However when I plug the ethernet into one of the Pi zero's ports and the power into the other, it still doesn't show up on the network. To be clear I plugged the ethernet straight from my router to the Pi zero and used the other port to power on the zero. With this setup I probed the network from my laptop and found no IP for the Raspberry Pi.

     

    That being said I wrote a little shell script to sleep 2m, then run the commands that you suggested I post the output of. Since I'm having trouble with the USB hub, I photographed the output of the three commands you suggested I try. They are as follows:

     

    imageimageimage

     

    A little unorthodox, I know, but it's the best I can think to do without the functional USB hub. Hopefully I'll have that new hub tomorrow or Monday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 10 years ago in reply to e14 Contributor

    It looks like you've got a (most likely static) IP - 10.0.0.30.

    What is your /etc/network/interfaces file contents?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    I have the same chipset  as you do. Mine did not work until I had enough power(amps) > 100 mA. I used the inside micro for Ethernet and not the outside one(it is power only).

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to shabaz

    Okay I see what you mean about the ip address, however when I try to ssh into 10.0.0.30 from my laptop the connection times out, and when I probe the network to see all active IP addresses 10.0.0.30 doesn't appear. Here is my /etc/network/interfaces file:

     

    image

     

    I have tried running dhcpcd eth0 but that hasn't solved the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    The power source shouldn't matter if I have the ethernet plugged straight into the Pi's inner usb port, correct? Thanks for trying the alternate method.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Yes that is true, unless the power supply to the Raspberry Pi zero is nominal in current. Can you get the actual voltage/amperage in front of zero?

    Thanks,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Yeah my power source is five volts and two amps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Yeah my power source is five volts and two amps.