Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Power Supply Pi3
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 757 views
  • Users 0 members are here
  • frontpage
  • raspberry_pi
Related

Power Supply Pi3

e14 Contributor
e14 Contributor over 10 years ago

Hi:

I'm getting that much closer to buying my Pi3. Never used one before. An absolute novice. My question is the power supply. The Officila Pi3 power adapter from raspberry.org says power supply sould be the official  5.1v 2.5A

MCM in the U.S. is selling one that is a 5V 2.4A. I live in the U.S.....which power supply it the correct one for me to buy? Kindly hel and Many Thanks.

Norman

  • Sign in to reply
  • Cancel
Parents
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    The 5.1V is to allow for a bit of loss in the cables and this will occure in situations where cheap USB wires are used. The official Adapter has a fixed cable that is excelent for the job. As clem57 has said, 2.4A covers added USB or Shields being added to the PI. If you are not doing this or using a powered USB Hub then a lower amperage adapter will still work. The cost of the official one is very good though so if you need to buy one, may as well go for the right one.

     

    The one I have (The official one in White), comes with adapters to suite most countries, the adapter itself will work for most countries based on 110V or 220/240V mains

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 10 years ago

    The 5.1V is to allow for a bit of loss in the cables and this will occure in situations where cheap USB wires are used. The official Adapter has a fixed cable that is excelent for the job. As clem57 has said, 2.4A covers added USB or Shields being added to the PI. If you are not doing this or using a powered USB Hub then a lower amperage adapter will still work. The cost of the official one is very good though so if you need to buy one, may as well go for the right one.

     

    The one I have (The official one in White), comes with adapters to suite most countries, the adapter itself will work for most countries based on 110V or 220/240V mains