Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Real Time DSP using the Cirrus Logic Card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 1972 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Real Time DSP using the Cirrus Logic Card

e14 Contributor
e14 Contributor over 10 years ago

I am looking at the Cirrus Logic card to act as the interface to do some audio DSP functions on a sample-by-sample basis in real time for SDR (Software Defined Radio).   Is this appropriate for the device?  It would have to run in a tight loop (preferably > 96 kHz):

   sample audio inputs --> process sample on the RPi in C language --> output on audio out  --> loop back.

I have not been able to find any user libraries for dealing with the card.  I would want it to loop as fast as possible.

 

I have the code working on a Arduino Due, but the 12-bit converters are marginal.

 

Thanks,

Derek

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    You want to process data not really audio. Right? I would try to use the Mali Videocore GPU on Raspberry Pi  instead since it is closer to the data source. It takes much time to send back and forth to a card depending on how much sent.

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    No, the signals are really audio (or at least in the audio bandwidth).   The two inputs will come in through the LINE-IN from the radio front-end.   They are IQ (quadrature) components of a waveform that will be decoded into audio by the RPi code, and played through the LINE-OUT.   The actual processing depends on the modulation (AM, FM, SSB, etc) of the radio signal.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Ok. Why not use a SDR dongle with antenna?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thanks Clem - we are kinda drifting away from my original question, but let me say that I have several SDR hardware systems around here, and many of the software packages - most of which use the PC sound card to to the DSP for modulation/demodulation.   Being a DIY sort of guy, I have been looking into using very small/inexpensive systems - for no particular reason.   As I said above, I have a complete Arduino Due based system working (capable of sampling at 1Msample/sec) but the 12 bit A/D and D/A limits the dynamic range.  The cycle time for a typical demodulator is around 20 usecs.  All DSP is done in integer arithmetic, and a lot of assembly code is used.

     

    I was hopeful that RPi 3 would let me do much better and the Cirrus Logic card looked like an ideal I/O system.  However, it seems that a lot of people are struggling with the drivers in Raspbian, and I am now wondering if there is any hope.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    And you are right about struggling with the Cirrus Logic card which is the same while Pi has improved. Why does so many overlook the HiFiberry system?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    And you are right about struggling with the Cirrus Logic card which is the same while Pi has improved. Why does so many overlook the HiFiberry system?

    Clem