Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Powering a PI (and accessories) from a 12v 15A rail.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 711 subscribers
  • Views 4365 views
  • Users 0 members are here
  • raspberry_pi
Related

Powering a PI (and accessories) from a 12v 15A rail.

halkun
halkun over 10 years ago

I'm getting together parts for a project that will put a Pi 3 with touch screen in my car. It's replacing the radio, but the 12v line that went to the radio has a 1A fuse, which is too low for the 2.4A power needed for the PI 3. However, under the radio is the cigarette lighter, which has a 15A fuse. Sadly, most of the 12v lighter to 5v USB adapters have a 1A limit. I'm going to need some kind of breakout that's going to power PI and it's various attachments.

 

Breaking down further -Things I need to power.

 

Raspberry Pi 3  - (5v 2.4A)

Touch Screen - ? (the pi powers it)

Pi Cam (Powered from Pi)

 

7 port USB hub (5v - 2A)

GPS module (Powers from USB hub)

External Webcam (Powers from USB hub)

 

What parts do you think will make something like this? I'll most likely be dong this in some perfboard. My guess is that I'll break out to:

-One USB (+5 and ground only @ 2.4 amps) to the  Pi/touchscreen complex and

-One wall wart "tube" power jack (5v  2A) to the USB hub.

 

Any ideas on a part list?

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 10 years ago

    The PI3 doesnt require 2.5A just can allow 2+ A throuogh to the USB peripherals.

    Use one of those adjutable Switch mode PSUs you can  get for aroun £1-2 each set the out put to 5V and glue it up...You are good to go then

     

    Also remember that 1 A at 12V is the same power as 2.4A at 5V so noting that those Regulators are 80-90% efficient you can draw 80-90% of that with out troubling the fuse anyway!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 10 years ago

    The PI3 doesnt require 2.5A just can allow 2+ A throuogh to the USB peripherals.

    Use one of those adjutable Switch mode PSUs you can  get for aroun £1-2 each set the out put to 5V and glue it up...You are good to go then

     

    Also remember that 1 A at 12V is the same power as 2.4A at 5V so noting that those Regulators are 80-90% efficient you can draw 80-90% of that with out troubling the fuse anyway!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer