Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Error Message Using Pi Camera Noire V2, but not when using PI Camera V2
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 3173 views
  • Users 0 members are here
  • raspberry_pi
  • pi noir v2
Related

Error Message Using Pi Camera Noire V2, but not when using PI Camera V2

e14 Contributor
e14 Contributor over 10 years ago

I've Raspberry Pi 3 B, with the latest version of NOOBS and install Raspbian. Has performed RPI-update, apt-get update and apt-get upgrade. When I plug the Pi Cam V2 everything works fine. Then I switch to Noir V2 (using the same ribbon, replace only cam) and get the following error message:

mmal: mmal_vc_comonent_enable: failed to enable comonent: ENOSPC

mmal: camera component could not be enabled

mmal: main: Failed to create camera component

mmal: Failed to run camera app. Please check for firmware updates

 

 

What should I do?

 

image

  • Sign in to reply
  • Cancel
Parents
  • therealmrchips
    0 therealmrchips over 10 years ago

    I am experiencing the EXACT same situation.  I am running a brand new V2 camera and a brand new V2 NOIR camera.  When I install the V2 camera on my Rpi3B, it works exactly as planned.  When I install the V2NOIR it gives the following error:

     

    mmal: mmal_vc_component_enable: failed to enable component: ENOSPC
    mmal: camera component couldn't be enabled
    mmal: main: Failed to create camera component
    mmal: Failed to run camera app. Please check for firmware updates

     

    Troubleshooting steps I have undertaken thus far:

     

    • Swapped cables on both cameras.  Both cables work fine with the V2 camera.  Neither one works on the V2NOIR.
    • Applied all the latest patches/firmware/updates.
    • From the StackExchange link: Modified the /boot/config.txt file to increase gpu_mem from 128 to 144 (even tried 256 just for kicks)
    • From the StackExchange link: Modified the /boot/cmdline.txt file to add the 1-Wire fix "bcm2708.w1_gpio_pin=18"
    • Checked and reseated the J2 connector between the NOIR camera itself and the board it is mounted on.
    • Swapped cameras onto a brand-new (different) Rpi3B board.  Same results (V2 Camera works, V2NOIR does not work - same errors).

     

    Anyone have any other suggestions?

     

    Thanks ahead of time!

     

    Rich

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to therealmrchips

    This is likely a hardware error. Read Rpi Camera Module - eLinux.org for some possible things to check.

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • therealmrchips
    0 therealmrchips over 10 years ago in reply to clem57

    Clem - You are correct.  It was a faulty device.  I returned it for a new one and that solved the problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • therealmrchips
    0 therealmrchips over 10 years ago in reply to clem57

    Clem - You are correct.  It was a faulty device.  I returned it for a new one and that solved the problem.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to therealmrchips

    Thanks. Kindly mark my response correct for others who may read.

    Cheers,

    Clem