Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 5 answers
  • Subscribers 712 subscribers
  • Views 4057 views
  • Users 0 members are here
  • raspberry pi
  • single-board
Related

Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?

e14 Contributor
e14 Contributor over 10 years ago

I'm not sure if anyone has really noticed or paid attention, but i have noticed ever since the single board computer has taken off (like the Raspberry pi) that they are mostly ARM based, why is that? I think it would be a lot easier if they were x86-x64 based, because it would be easier to use programs that you are used to using instead of finding ARM versions.

  • Sign in to reply
  • Cancel
Parents
  • uscdadnyc
    0 uscdadnyc over 10 years ago

    To Robert Wolff & the others:

    I have any old RaspPi Mod 1B which I mounted on an Old USB 1.1  powered Hub (b/c this was circa 2013). I use it in conjunction w/ MOOC courses. A Python Course at coursera.edu and a H/W course at udemy.com. A whole different world from my x86 Toys. I bought a Intel NUC5i7RYH for about $500 (barebones) this in contrast to the $35 RaspPi. I tricked-out the NUC w/ 16GB Ram and an M.2 256GB SSD (which died) now running on a 2.5" 480GB SSD. Win10 comes up in 11 seconds. Different Worlds/Functions, RaspPi for dabbing in H/W. x86/windows for High-powered Stuff. Although Intel is trying to get into the SOC market(?). isn't it Microsoft that is making a Push (on the s/w side) with their Win10-IOT (Not full-fledged Win10)?

    BTW Thx to all comment-ers on bring me down Memory Lane.

    USCDADNYC (NY NY)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to uscdadnyc

    That is a true state of affairs in this world even today. Facts do stnd the test of time where as fiction comes and goes.

    Thanks for your assessments!

    C

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago in reply to uscdadnyc

    That is a true state of affairs in this world even today. Facts do stnd the test of time where as fiction comes and goes.

    Thanks for your assessments!

    C