Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 5 answers
  • Subscribers 712 subscribers
  • Views 4060 views
  • Users 0 members are here
  • raspberry pi
  • single-board
Related

Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?

e14 Contributor
e14 Contributor over 10 years ago

I'm not sure if anyone has really noticed or paid attention, but i have noticed ever since the single board computer has taken off (like the Raspberry pi) that they are mostly ARM based, why is that? I think it would be a lot easier if they were x86-x64 based, because it would be easier to use programs that you are used to using instead of finding ARM versions.

  • Sign in to reply
  • Cancel
Parents
  • johnbeetem
    0 johnbeetem over 10 years ago

    My two answers: cost and heat.  ARM processors are a lot cheaper than x86 processors.  ARM's business model is to license the ARM architecture and/or implementations rather than make the chips themselves.  Licencees like TI, NXP/Freescale, Broadcom, Qualcomm, Allwinner, and many others compete with each other to sell the cheapest chips.  ARM's license fees are modest which keeps the chips cheap.

     

    ARM SoCs are designed for very high volume mobile products.  High volume drives the prices down.

     

    From the beginning ARM pushed low power.  Intel has pushed processor performance by fitting as many fast transistors as possible onto a piece of silicon.  Power consumption has always been secondary to speed.  Low power is why ARM is the best choice for mobile devices, where you want the battery to last as long as possible.

     

    Most single-board computers are very small.  If you try to pack high power chips on a small board you end up with heat issues (like poor reliability) and need to add cooling devices.

     

    A lot of people who do embedded programming already use GNU/Linux and other open-source software on their development PCs.  When you have source code, targeting ARM instead of x86 is no big deal.

     

    JMO/YMMV

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 10 years ago in reply to johnbeetem

    Ironically, Intel's acqisition of Altera (who I believe has ARM core capability) might just make Altera ARM implementations the fastest, lowest power ARM chips on the market, because Intel's fine-geometry IC technology is at the leading edge for speed and power consumption. I'm not quite sure ARM technolgy is automatically scalable to Intel's IC process or if ARM themselves need to design for the finer geometry process.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 10 years ago in reply to johnbeetem

    Ironically, Intel's acqisition of Altera (who I believe has ARM core capability) might just make Altera ARM implementations the fastest, lowest power ARM chips on the market, because Intel's fine-geometry IC technology is at the leading edge for speed and power consumption. I'm not quite sure ARM technolgy is automatically scalable to Intel's IC process or if ARM themselves need to design for the finer geometry process.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to dougw

    Douglas Wong wrote:

     

    Ironically, Intel's acquisition of Altera (who I believe has ARM core capability) might just make Altera ARM implementations the fastest, lowest power ARM chips on the market...

    Intel has had an ARM architectural license ever since they bought the StrongARM technology from Digital Equipment Corporation in 1998.  Intel tried to sell communications chips based on an ARM version called XScale but I don't think it got anywhere.  Intel sold most of their ARM technology to Marvell in 2006.

     

    For more detail, see XScale at Wikipedia.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to johnbeetem

    And Marvel applied the ARM technology to their controllers, etc.