Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 5 answers
  • Subscribers 712 subscribers
  • Views 4058 views
  • Users 0 members are here
  • raspberry pi
  • single-board
Related

Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?

e14 Contributor
e14 Contributor over 10 years ago

I'm not sure if anyone has really noticed or paid attention, but i have noticed ever since the single board computer has taken off (like the Raspberry pi) that they are mostly ARM based, why is that? I think it would be a lot easier if they were x86-x64 based, because it would be easier to use programs that you are used to using instead of finding ARM versions.

  • Sign in to reply
  • Cancel
Parents
  • rew
    0 rew over 10 years ago

    Many embedded processors are ARM processors. They are better suited for embedded stuff. One of the things is that they get more computing work done per unit of energy consumed. Secondly, there are many "system on a chip" (SOC for short) ARM processors. Like the BCM2735. That integrates lots of peripherals into the chip so that you don't need extra chips. So take a look at the raspberry pi zero... You have a single board computer there with HDMI output, a storage interface and half a gigabyte of RAM. All in that single black blob in the middle!

     

    Intel has been trying to get "in on the action" for over a decade now. They haven't been really successful, because their processors require too much support hardware around them, meaning the boards get big and expensive. So for example: https://azerty.nl/0-843-709774/intel-next-unit-of-computing-board-de3815tybe-moederbord-ucff-intel-atom-e3815-usb-3-0-gi… which doesn't even have RAM but is 4x more expensive than a raspberry pi. And it requires a bigger powersupply. (in my quick search for something like this, I found a EUR 73 board, but that was just the breakout for another intel board....)

     

    The cheapest Intel CPUs come in at around EUR 40. extreme low-end ones maybe half that.... An ARM CPU can be bought for 32 cents! Ok, that's a low-end ARM V6...... hmm... just like the raspberry pi (1). OK, that one doesn't have everything the raspberry pi CPU has, but it can be bought for way less than $1 in low quantities. At higher quantities the raspberry pi CPUs apparently also cost only $1-$2. The RAM is probably similar, and they sell at $5 (for the zero).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rew
    0 rew over 10 years ago

    Many embedded processors are ARM processors. They are better suited for embedded stuff. One of the things is that they get more computing work done per unit of energy consumed. Secondly, there are many "system on a chip" (SOC for short) ARM processors. Like the BCM2735. That integrates lots of peripherals into the chip so that you don't need extra chips. So take a look at the raspberry pi zero... You have a single board computer there with HDMI output, a storage interface and half a gigabyte of RAM. All in that single black blob in the middle!

     

    Intel has been trying to get "in on the action" for over a decade now. They haven't been really successful, because their processors require too much support hardware around them, meaning the boards get big and expensive. So for example: https://azerty.nl/0-843-709774/intel-next-unit-of-computing-board-de3815tybe-moederbord-ucff-intel-atom-e3815-usb-3-0-gi… which doesn't even have RAM but is 4x more expensive than a raspberry pi. And it requires a bigger powersupply. (in my quick search for something like this, I found a EUR 73 board, but that was just the breakout for another intel board....)

     

    The cheapest Intel CPUs come in at around EUR 40. extreme low-end ones maybe half that.... An ARM CPU can be bought for 32 cents! Ok, that's a low-end ARM V6...... hmm... just like the raspberry pi (1). OK, that one doesn't have everything the raspberry pi CPU has, but it can be bought for way less than $1 in low quantities. At higher quantities the raspberry pi CPUs apparently also cost only $1-$2. The RAM is probably similar, and they sell at $5 (for the zero).

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer