Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 21 replies
  • Answers 5 answers
  • Subscribers 712 subscribers
  • Views 4055 views
  • Users 0 members are here
  • raspberry pi
  • single-board
Related

Why is it that most Single-board computers are based off the ARM chipset instead of x86-x64?

e14 Contributor
e14 Contributor over 10 years ago

I'm not sure if anyone has really noticed or paid attention, but i have noticed ever since the single board computer has taken off (like the Raspberry pi) that they are mostly ARM based, why is that? I think it would be a lot easier if they were x86-x64 based, because it would be easier to use programs that you are used to using instead of finding ARM versions.

  • Sign in to reply
  • Cancel
Parents
  • DAB
    0 DAB over 10 years ago

    Hi Matthew,

     

    A little bit of history can answer your question.

    When the MCU market exploded, 8 bit computers became the de facto standard for embedded systems.

    In the 1970's there were many SBC kits for engineers to learn about embedded systems and to explore potential applications.

     

    Through the 1990's most embedded applications used 4 bit and 8 bit processors.  Intel was the major player in this world as well as the PC world, so while they had some support for the 8086 architecture, they had little reason to add specific embedded capability to the product line.

     

    All of that changed after 2000 with the surge in smart phones, devices and consumer electronics.

    Manufacturers needed to pack more capability into their chips than just the processor and some memory.

    ARM came into that environment with an easy to use System On A Chip (SOC) architecture that they could easily put standard display and IO components plus enough memory to shrink the chip count dramatically.

     

    Initially, these applications were small runs compared to the PC level devices, so Intel just did not see a good market to invest the 8086 architecture for those types of applications.

     

    Fast forward to the present and Intel now sees that they missed the leading edge of an entire business area and are now playing catch up.

     

    There is no architecture advantages inherent with the 8086 architecture to move it into this product space.

     

    So here we sit today with a few companies advancing along the ARM architecture and some others.

    At this point, the level of support dictates the cheapest path, which is the ARM environment, especially with the open source support and freeware available.

     

    For Intel to compete, they need a large investment and time, both of which the competition now has a huge advantage.

     

    So I would not look for an 8086 type MCU in the future.

    I would expect a leap in technology out of Intel so that they can run past the competition rather than play catch up.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 10 years ago

    Hi Matthew,

     

    A little bit of history can answer your question.

    When the MCU market exploded, 8 bit computers became the de facto standard for embedded systems.

    In the 1970's there were many SBC kits for engineers to learn about embedded systems and to explore potential applications.

     

    Through the 1990's most embedded applications used 4 bit and 8 bit processors.  Intel was the major player in this world as well as the PC world, so while they had some support for the 8086 architecture, they had little reason to add specific embedded capability to the product line.

     

    All of that changed after 2000 with the surge in smart phones, devices and consumer electronics.

    Manufacturers needed to pack more capability into their chips than just the processor and some memory.

    ARM came into that environment with an easy to use System On A Chip (SOC) architecture that they could easily put standard display and IO components plus enough memory to shrink the chip count dramatically.

     

    Initially, these applications were small runs compared to the PC level devices, so Intel just did not see a good market to invest the 8086 architecture for those types of applications.

     

    Fast forward to the present and Intel now sees that they missed the leading edge of an entire business area and are now playing catch up.

     

    There is no architecture advantages inherent with the 8086 architecture to move it into this product space.

     

    So here we sit today with a few companies advancing along the ARM architecture and some others.

    At this point, the level of support dictates the cheapest path, which is the ARM environment, especially with the open source support and freeware available.

     

    For Intel to compete, they need a large investment and time, both of which the competition now has a huge advantage.

     

    So I would not look for an 8086 type MCU in the future.

    I would expect a leap in technology out of Intel so that they can run past the competition rather than play catch up.

     

    DAB

    • Cancel
    • Vote Up +4 Vote Down