Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi (camera) flex cable converter
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 2 answers
  • Subscribers 708 subscribers
  • Views 4570 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Pi (camera) flex cable converter

e14 Contributor
e14 Contributor over 10 years ago

Hi,

I'm starting to use the Rpi with the camera module.

I want to hook up many camera modules to one RPI but the flex cable between them is rather unuserfriendly, I need to remove it many times.

So, I'm looking for a connector to convert the flex cable to another type on connector like HDMI.

The schematic would look like this:

RPI---flex cable -- HDMI_female --- HDMI_male --- flex cable -- camera module.

Instead of HDMI, another type of connector is also welcome. It must be disconnected really quickly,

 

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • gdstew
    0 gdstew over 10 years ago

    Try googling  raspberry pi camera hdmi for other solutions

     

    https://www.tindie.com/products/freto/pi-camera-hdmi-cable-extension/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to gdstew

    Hi,

    this is very helpfull !! I will look at it.

    thank you for your help.

     

    Regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    As expected the "cam_ext" kit also works for the 8Mpixel camera. I currently tested "80cm" as "working" and close to 3m as "not working". Apparently the limit in the distance is lower for the 8Mpixel version than for the 5Mpixel one.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    As expected the "cam_ext" kit also works for the 8Mpixel camera. I currently tested "80cm" as "working" and close to 3m as "not working". Apparently the limit in the distance is lower for the 8Mpixel version than for the 5Mpixel one.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to rew

    Not surprising when you consider more data at 8M pixels have to travel in a certain finite time. Thanks for the test rew

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rew

    Roger,

    I thought that the IDC flatcable must be shorter than in case of a 5Mp camera. The speed is higher for 8Mp.

    Maybe a shielded cable can be longer? But maybe 80cm is more than enough.

    Anyway, thank you very much for the test.

     

    Regards.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to e14 Contributor

    Modern "fast" signals commonly travel over "differential pairs". USB at 12 Mbps started that, but SCSI at 20-40 MHz and higher probably already existed at that time. Nowadays this trick works up to signals in the Gbps range.


    When a sata cable is say 60 cm long and you're doing 6 Gbps, the light speed dictates that around 12 bits are simply "in transit" ON THE CABLE! In reality it is about twice as many! (between 18 and 36 bits are in transit on the cable!)

     

    This requires that the waveform of the signal coming out quite much resembles what went in at the other side. This is possible with differential pairs. That's why the important signals on the small flatcable but also on our extension kit are still next to each other: to make a differential pair.

     

    But it also means that it doesn't really matter much how long the cable is.... The cable doesn't care if there is two, five, or ten

     

    That remark of course isn't true: there are some losses and hopefully they are small enough so that the receiving end still can decode the signals. So.... It is the losses in the cable, that mean that the bits don't come through. Not the fact that the first bit has to have arrived before the next one can be sent.

     

    Until further notice, we won't ship "cam ext" kits with a longer than 80 cm cable. This until I get the chance to test a few "in between" lengths.