Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Connect a Raspberry 2/3 Board to the compute io board
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 838 views
  • Users 0 members are here
  • compute module development kit
  • raspberrypi.
  • can bus
  • gpio pinout
  • raspberry_pi
Related

Connect a Raspberry 2/3 Board to the compute io board

e14 Contributor
e14 Contributor over 10 years ago

I want to connect the CAN-Module Pican 2 (http://skpang.co.uk/catalog/pican2-canbus-board-for-raspberry-pi-23-p-1475.html ), which is developed for the Raspberry 2/3, to the Compute CMIO.

 

How can I map the gpio pins right or is the order the same on the Raspberry PI 2/3 to the Compute IO Board?

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    You are free to use banks 0&1, but bank 2 is reserved for the eMMC.

    BCM283x has 3 banks of General Purpose Input Output (GPIO) pins (28 pins on Bank0, 18 pins on Bank1 and 8 pins on Bank2; 54 pins in total). These pins can be used as true GPIO (i.e. software can set them as inputs or outputs, read and/or set state and use them as interrupts) but also can be set to 'alternate functions' such as I2C, SPI, I2S, UART, SD card and others.

    From: https://www.raspberrypi.org/documentation/hardware/computemodule/cm-peri-sw-guide.md .

     

    If you have the kit, no problem to use the pins. But they are not the same as the other Pi's. Read https://www.raspberrypi.org/documentation/hardware/computemodule/ for full details. You may want to download https://www.raspberrypi.org/documentation/hardware/computemodule/RPI-CMIO-V1_2-PUBLIC.zip

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    So I connected the board to the compute module, but I think the overlay-file is not working because the SPI is not configured in the right way.

    Is there a working overlay file for spi0?

    Currently I tried to work with the spi-bcm2835-overlay but the SPI is not really working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 10 years ago in reply to e14 Contributor

    I don't want to muddy the waters any further(especially when IDK[I Don't Know what I am talking about But the acronyms being referred to w/o attribution/explanation makes it hard for a Novice like me to follow AAR Thx for you(guys/gals's Posts IDK there was a"BUSS called the Can-Bus I guess used in automotive system Now if I see a DB-9 Connector in a Car/Lorry(UK I will know that it is NOT a stripped-down version of the 25pin DB-25 Connector used in the old  RS-232RS-232 of yesteryear BTW in my cursory look on the Internet on the Terms used here I ran across this URL

    Raspberry Pi Bootloader License Precludes it to Run on Competing Broadcom BCM283x Boards

    IDK whether it is applicable OR Not. Sorry about my intrusion.

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer