Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Additional SPI slave
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 2 answers
  • Subscribers 707 subscribers
  • Views 1127 views
  • Users 0 members are here
  • spi
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Additional SPI slave

hiroolt
hiroolt over 10 years ago

Hi,

 

I'm using CLAC with raspberry pi 3, and it works well. (Linux raspberrypi 4.4.6-v7+, cirrus-linux-4.4.6).

As a next step, I'm trying to add one more SPI slave somehow in order to use mcp3008.

But SPI1 pins (GPIO 18-21) are occupied by I2S functions which are used by CLAC,

and I'm not sure if I could add SPI0.2 by modifying "rpi-cirrus-wm5102.dts".

 

Could anyone kindly tell me how to add additional SPI slaves?
#Should I use I2C ADC?

 

Thanks,

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    Depends how often you use the CLAC at the same time as the MCP3008. If you use both nearly at the same time, I would use software SPI.

    The MCP3008 connects to the Raspberry Pi using a SPI serial connection.  You can use either the hardware SPI bus, or any four GPIO pins and software SPI to talk to the MCP3008.  Software SPI is a little more flexible since it can work with any pins on the Pi, whereas hardware SPI is slightly faster but less flexible because it only works with specific pins.  If you aren't sure which to use I recommend software SPI as it's easier to setup.
    From: https://learn.adafruit.com/raspberry-pi-analog-to-digital-converters/mcp3008

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • hiroolt
    0 hiroolt over 10 years ago in reply to clem57

    Hi Clem,

     

    Thanks you for your prompt reply.

    I don't need frequent access to the device (less than once/sec), so your suggestion would be perfectly suitable for me.

    Thanks!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • hiroolt
    0 hiroolt over 10 years ago in reply to clem57

    Hi Clem,

     

    Thanks you for your prompt reply.

    I don't need frequent access to the device (less than once/sec), so your suggestion would be perfectly suitable for me.

    Thanks!!