Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using 4-pin Ethernet on the Pi 3?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 709 subscribers
  • Views 2517 views
  • Users 0 members are here
  • ethernet
  • raspberry pi 3
Related

Using 4-pin Ethernet on the Pi 3?

e14 Contributor
e14 Contributor over 10 years ago

Hey everyone. Just bought a Pi 3 recently. I am trying to use the 10/100 Ethernet on the Pi, but the cable I am using is a four wire cable. 10/100 should only use 4 pins, however, so this shouldn't be a problem. My MacBook can use the internet fine with this cable, but the Pi fights with me. When plugged in, the green light on the port flashes quickly, continuously, and my router never seems to assign the Pi an IP. The Pi shows no signs of an outgoing connection, either, even though my terminal says that it recognizes the 10/100 link has been connected.

 

Any reason the 4 pin ethernet isn't working? And possible solution? The cable actually has six wires, but I have only connected the four used in 10/100 ethernet wiring.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 10 years ago

    If the cable is RJ45 it usually has 8 wires connected. See RJ45 Wiring Diagram for Ethernet where they are coded. In actual usage only 2 pairs are needed. May sure we are not using RJ11 (4 wire) as in Wiring Termination Instructions and Diagrams - RJ11 and RJ45 Jacks Guide ,,,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago

    If the cable is RJ45 it usually has 8 wires connected. See RJ45 Wiring Diagram for Ethernet where they are coded. In actual usage only 2 pairs are needed. May sure we are not using RJ11 (4 wire) as in Wiring Termination Instructions and Diagrams - RJ11 and RJ45 Jacks Guide ,,,

    Clem