Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Using 4-pin Ethernet on the Pi 3?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 709 subscribers
  • Views 2517 views
  • Users 0 members are here
  • ethernet
  • raspberry pi 3
Related

Using 4-pin Ethernet on the Pi 3?

e14 Contributor
e14 Contributor over 10 years ago

Hey everyone. Just bought a Pi 3 recently. I am trying to use the 10/100 Ethernet on the Pi, but the cable I am using is a four wire cable. 10/100 should only use 4 pins, however, so this shouldn't be a problem. My MacBook can use the internet fine with this cable, but the Pi fights with me. When plugged in, the green light on the port flashes quickly, continuously, and my router never seems to assign the Pi an IP. The Pi shows no signs of an outgoing connection, either, even though my terminal says that it recognizes the 10/100 link has been connected.

 

Any reason the 4 pin ethernet isn't working? And possible solution? The cable actually has six wires, but I have only connected the four used in 10/100 ethernet wiring.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    So the cable is actually quite long. It is, to my understanding, Cat 5e cable that is running through the walls of my house. However, the brown and brown/white wires are missing from the cable. I have no real way of telling how long the cable actually is, but I would guess around 200ft. I know this length is fine as I have created ethernet cables that can run further. The wiring in the wall must be done at least somewhat correctly as my Mac can use it at the full 90 Mbits my ISP provides.

     

    I read something online about the Pi's ethernet port being wired incorrectly or cheaply or something along those lines, but it was mostly people talking about PoE which I don't need.

     

    Clem, the ending jacks are definitely RJ45 jacks; I just only have 6 wires to work with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    So the cable is actually quite long. It is, to my understanding, Cat 5e cable that is running through the walls of my house. However, the brown and brown/white wires are missing from the cable. I have no real way of telling how long the cable actually is, but I would guess around 200ft. I know this length is fine as I have created ethernet cables that can run further. The wiring in the wall must be done at least somewhat correctly as my Mac can use it at the full 90 Mbits my ISP provides.

     

    I read something online about the Pi's ethernet port being wired incorrectly or cheaply or something along those lines, but it was mostly people talking about PoE which I don't need.

     

    Clem, the ending jacks are definitely RJ45 jacks; I just only have 6 wires to work with.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    See Not All Ethernet Cables Are Equal: You Can Get Faster LAN Speeds By Upgrading . What is your CAT rating?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 10 years ago in reply to e14 Contributor

    I would first try the RasPi 3 with a short Ethernet cable just to make sure its Ethernet port works at all.  If that's the case, it's probably that your long Ethernet cable through the walls is slightly flaky and it may work or not depending on how well the PHY chips at each end adapt to an iffy cable.

     

    Another possiblity is that RasPi's Ethernet jack is making poor contact on one pin.  Ethernet uses differential pairs.  If one side of the pair is broken, you can often get enough signal through the other side to get some level of connectivity, but it's really unreliable.  Do a visual check to see that all the pins look good.

     

    If you have a spare Ethernet switch lying around, try putting it between the RasPi 3 and your long cable.