Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum can the pi 3 control wifi power?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 706 subscribers
  • Views 950 views
  • Users 0 members are here
  • raspberry_pi
  • rasberry pi 3
  • wi-fi;
Related

can the pi 3 control wifi power?

e14 Contributor
e14 Contributor over 10 years ago

Hi all,

 

I am architecting a project in which it will be helpful to control the radio power of the WiFi on the Pi 3.  Can this be done?

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 10 years ago

    In general the answer is yes, but it depends on the Linux you have installed and chip driver capabilities.. See https://wireless.wiki.kernel.org/en/developers/documentation/ieee80211/power-savings  for a discussion.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thanks for jumping in, Clem.  I genuinely appreciate.

     

    And forgive me but I'm not sure I was entirely clear.  I am not concerned with saving power but with actually reducing the broadcast power of the WiFi radio.  The application I'm architecting operates in a very small area, and the design of the associated hardware elements may be simplified if I can actually reduce the broadcast power of the WiFi radio on the Pi 3 board.

     

    Of course if I simply missed that in the pointer you sent me, please point out what a dolt I am.  I never mind being corrected.

     

    And thanks again for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to e14 Contributor

    Here is the details of the Broadcom wireless chip in Raspberry Pi 3 in http://www.cypress.com/file/298076/download . There are a few sections mentioning the power management feature. Beware that although the chip may do these things, the driver code in the OS may or may not support such features like I stated above. Especially since this is new chip. I would consider maybe using your own wireless solution if this proves to be not supported at this time. Sorry for long winded answer.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to clem57

    Thank you again, Clem, for this pointer.  I'm going through the specs now, and if between the Cypress/Broadcomm chip and the OS broadcast power is not manageable, I'll certainly be following your suggestion and using my own wireless solution.

     

    Sheldon