Products
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
Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi 3 No audio through HDMI
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 1 answer
  • Subscribers 707 subscribers
  • Views 31396 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Raspberry pi 3 No audio through HDMI

e14 Contributor
e14 Contributor over 10 years ago

I need some help fixing the audio so it comes out through the HDMI cable. Also how do I reboot?

  • Sign in to reply
  • Cancel
  • ghaberek
    0 ghaberek over 10 years ago

    The Raspberry Pi should output audio through the HDMI connector automatically.

     

    There is an article here that describes how to manually configure the audio output: Audio configuration.

     

    You may be running into the issue described at the bottom of the page:

    If you're still not getting sound via HDMI

    In some rare cases, it is necessary to edit config.txt to force HDMI mode (as opposed to DVI mode, which does not send sound).

    You can do this by editing /boot/config.txt and setting hdmi_drive=2, then rebooting for the change to take effect.

    You can reboot by clicking Menu > Log off.. or open a terminal and type sudo reboot.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to ghaberek

    Thanks for advice. I was able to get the audio working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gleandre
    0 gleandre over 9 years ago in reply to e14 Contributor

    so how was you able to resolve the  problem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • velicusimon
    0 velicusimon over 7 years ago in reply to gleandre

    I've tried every solution in here and i couldn't get the HDMI audio to work. I gave up and put all the options back to how they came by default but then i've found out that when I play an audio file using this command: omxplayer -o both file.mp3, the audio was working so i've decided to give it one more try and i've finally found the solution. None of the things in the config file will affect your audio so i think the best way is to put them back as they were by default and then open a console and do exactly this:

     

     

     

     

    sudo apt-get remove --purge alsa-utils*

    sudo apt-get clean

    sudo apt-get autoremove

    sudo apt-get remove --purge alsamixer*

    sudo apt-get clean

    sudo apt-get autoremove

     

     

    sudo apt-get update

    sudo apt-get upgrade

     

     

    sudo apt-get install alsa-utils

    sudo apt-get install alsamixer

     

     

    sudo reboot

     

     

    Then select the HDMI output using the speaker icon in the taskbar and that's it. I hope it works for you !

     

     

    I've been able to find out this solution because of the omxplayer (that worked) which is a very basic music player that doesn't use the alsa driver, instead it has it's own drivers named openmax, so the problem had to be coming from the alsa drivers.

     

     

    *IF IT'S STILL NOT WORKING AFTER DOING WHAT I'VE SAID ABOVE, than you could also try to uncomment hdmi_drive=2 in /boot/config.txt to force HDMI mode. (To do this you have to open up a console, write sudo nano /boot/config.txt and the file will open, navigate down to hdmi_drive and delete the # that's before it then hit Ctrl+X, hit Y and enter then enter once again. After that reboot the system and prey :))

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rwadeg
    0 rwadeg over 7 years ago

    This worked on Raspberry Pi 4 using noobs 3.2.0 on 8/9/2019

     

    Open a terminal

     

    type: sudo leafpad

     

    In leafpad click 'file' then click 'open' on the drop down menu

     

    now click 'File System'

     

    Double click 'boot'

     

    Find the file 'config.txt' and open it

     

    go down a few lines in 'config.txt' and find '#hdmi_drive=2'

     

    Remove the '#' so it reads 'hdmi_drive=2'

     

    Save changes and exit leafpad

     

    Reboot system and sound should work. It worked for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • discobiscuit
    0 discobiscuit over 6 years ago

    Using this command in the console worked for me:

    amixer cset numid=3 2

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • colporteur
    0 colporteur over 6 years ago

    Any chance you can share some details from your problem?

     

    What Pi hardware are you using?

    What operating system are you using?

    What was the HDMI problem you were experiencing?

    How did you resolve the problem?

     

    I found HDMI audio output pretty stable. When someone has an issue, there is usually something they have done or are trying to do. There is also a new release of Raspbian operating system just released. If your HDMI audio issues exists with this O/S it may be something systemic that we can all learn from.

     

    Care to share?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Zakkg3
    0 Zakkg3 over 3 years ago

    Just right click on the speaker and select HDMI solved it for me.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • TekMaker
    0 TekMaker over 3 years ago

    sudo reboot 

    that will do it

    • Cancel
    • Vote Up -2 Vote Down