Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum NesPi Needs More Power
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 26 replies
  • Answers 3 answers
  • Subscribers 709 subscribers
  • Views 4788 views
  • Users 0 members are here
  • nespi power
  • raspberry_pi
Related

NesPi Needs More Power

e14 Contributor
e14 Contributor over 10 years ago

So i am doing the nespi project and have found that i need power to a usb hub and power to the pi. I only have installed one usb 3.0 port for power to come into the nes case. If i get this power supply --> https://www.amazon.com/Adapter-Portable ... wer+supply

 

Can i take two usb cables from ^^^this power supply from a usb splitter into a single usb cable then split it back out into two usb connections. Then have one end go to the pi and the other end go to the usb hub to power both devices.

 

Another possibility i have thought of is trying to bring more amps to the usb hub but i do not know it it can handle more power in and if that would allow it to output more power per port.

 

I would also greatly appreciate any other ideas on how to get power to both devices with only using one usb port to get power into the case.

 

Attached is the setup before the powered usb hub was added in to power the 4 controllers separate from the pi's power. And the back port is the single usb 3.0 port i have to bring power into the case.

 

Hopefully later i can get a pic of that to help with any questions on the setup.

Attachments:
image
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    i Tried that once and could not get enough power to the pi with a 5v 3 amp power supply.

     

    when i tested ^^^ this i had 3 amps coming  into the hub then 2 controllers in the hub and the pi on the hub. i then had 2 controllers off the pi and a jump drive. With all this plugged in the 3 amp power supply could not get enough power to it. I am going to try a cable similar to the link you posted but for usb only and hope a single usb cable wont bottleneck it to bad. Going this route it should have around 4 amps coming it. If i use a 24watt anker dual usb charger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    i Tried that once and could not get enough power to the pi with a 5v 3 amp power supply.

     

    when i tested ^^^ this i had 3 amps coming  into the hub then 2 controllers in the hub and the pi on the hub. i then had 2 controllers off the pi and a jump drive. With all this plugged in the 3 amp power supply could not get enough power to it. I am going to try a cable similar to the link you posted but for usb only and hope a single usb cable wont bottleneck it to bad. Going this route it should have around 4 amps coming it. If i use a 24watt anker dual usb charger.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • uscdadnyc
    0 uscdadnyc over 10 years ago in reply to e14 Contributor

    AM wrote>>...i Tried that once [use a BIG cable] and could not get enough power to the pi with a 5v 3 amp power supply...

    USCDADNYC reply>>IDK (I Don't Know) if you are unfamiliar/adverse-to "Soldering/wiring" your own "Jerry-rig" solution. But if that picture (...134001.jpg) shows the HDMI and USB3.0 Receptacles AND the USB3.0 WILL BE USED FOR DC POWER ONLY. You might want to re-purpose the Pins in the USB3.0 Receptacle. BUT THIS IS DANGEROUS! Do a wiki on "USB" and check-out how many conductors are on a USB 3.0 Receptacle. You could re-purpose some of these wires to carry (separate USB Brick PSU's Voltages). On the inside you could split the USB3.0 wires back into separate USB Brick PSU Vdc voltages. TIP: if you have any (a) BAD/DEFECTIVE PC MoBo's (MoBo = Motherboards) and (b) a Dremel Tool. you can cut those stacked USB2.0 Ports OFF the MoBo And use these inside your Box. Then on the Outside you would have to cut-up a USB3.0 Cable and splice the appropriate wiring from two (or more) USB Brick PSU's. Think of your mounted USB3.0 Receptacle as a "FUNNEL" to get Power into your Box. If you do this, BE SURE to LABEL the USB3.0 Receptacle as "NON-STANDARD". Of course if any of your MI Force (MI = Mission Impossible) should get caught, the Secretary (USCDADNYC) will disavow any of your actions. Also keep in mind: Caveat Emptor. And Assumption of the Risks.

    To RW: Your referred to an alibaba site. Are along the Pacific Rim? (physically)

    USCDADNYC (NY NY USA)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 10 years ago in reply to uscdadnyc

    RW is me? Call me "REW" on forums... :-)

    No, I'm in the Netherlands.... Western Europe.

    Some people don't dare buy stuff off ebay/aliexpress/alibaba because they got burned once. Fine.

     

    But with some care, you can get good stuff at great prices from there. Sometimes you get something you didn't expect. So somehow I got good probes for my multimeter. So I wanted them again for my other multimeters. I order them, and I get "scale models". They look exactly the same, just at 80% scale. In that case, I was lucky: the seller had mentioned the size of the product in the offer, and that corresponded to what I already had. Got an "oops sorry, here are the correct ones".

    Another thing people fall for is that they buy stuff that has specs that most people can't verify easily. Like batteries or powerbanks. There you are likely to get 10 times less capacity than claimed!
    But the leds I ordered yesterday are pretty good. How much current do most people push through a led? 20mA? They still glow visibly at 60nA. That's 300 thousand times less current than allowed. You need to look carefully to see that, but at 20uA they function great as indicator lights.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer