Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum what battery do i need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 1790 views
  • Users 0 members are here
  • nimh
  • portable pi
  • help
  • battery
  • raspeberrypi
  • question
Related

what battery do i need?

vinceverc
vinceverc over 9 years ago

So i want to buld a raspberry pi portable. I am new to electronics and have a question.

It has to have a built in display and i will probably just connect a keyboard to it to configure it.

And i would like to give it a tablet like shape and just connect a usb mouse (I would also like to make it this way so i do not need a keyboard when using it, because it is portable and the mini keyboards cost a lot)

I found a backup display on amazon wich is 7 inches and needs 12v and 5 Wats

The raspberry pi needs 5 volts at 2.5 amps

So my question is: what battery do i need?

I watched a video about the types and i am going with a NiMH battery because the video said it was safe.

But what kind of ratings do i need?

Do i need a 17v battery and put the screen and pi in series, or do i fry something then?

And how di charge it? do i have to take out the battery when charging or can i connect the pi and screen to the charging circuit or something?

please help and sorry for this stupid question.

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Vincent,

     

    It would be easier to use a display which also requires the same voltage (5V), so you can run both the Pi and the display from a single 5V source. There are USB power sources (they have Li-Ion cells inside) with a USB output of 5V (there is an in-built DC-DC converter) which are intended for charging mobile phones. They can be used to power the Pi and display (you don't need 10V, the Pi and display are wired in parallel).

    Also, the car reversing/backup displays are low-res, it may be hard to make out any text if it was used as a tablet. Some state a high res but actually output a standard def image which is unusable for text. About the minimum would something like the Pi 7" capacitive touch display, or some HDMI display perhaps.

    Also, it would be good to check out some existing projects like this, for ideas, e.g. this URL: https://learn.adafruit.com/7-portable-raspberry-pi-multitouch-tablet/overview

    You're right to be concerned about safety (that URL unfortunately does not mention battery safety, and I'm not sure I'd use a zip-tie around a Li-Po cell. But the rest of the info may be useful there), the off-the-shelf 5V USB power packs should be safe if some known reputable one is used (check the reviews on Amazon etc) from a reputable source. Make sure it can supply perhaps 2A or more (the Pi and display may consume this much).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Vincent,

     

    It would be easier to use a display which also requires the same voltage (5V), so you can run both the Pi and the display from a single 5V source. There are USB power sources (they have Li-Ion cells inside) with a USB output of 5V (there is an in-built DC-DC converter) which are intended for charging mobile phones. They can be used to power the Pi and display (you don't need 10V, the Pi and display are wired in parallel).

    Also, the car reversing/backup displays are low-res, it may be hard to make out any text if it was used as a tablet. Some state a high res but actually output a standard def image which is unusable for text. About the minimum would something like the Pi 7" capacitive touch display, or some HDMI display perhaps.

    Also, it would be good to check out some existing projects like this, for ideas, e.g. this URL: https://learn.adafruit.com/7-portable-raspberry-pi-multitouch-tablet/overview

    You're right to be concerned about safety (that URL unfortunately does not mention battery safety, and I'm not sure I'd use a zip-tie around a Li-Po cell. But the rest of the info may be useful there), the off-the-shelf 5V USB power packs should be safe if some known reputable one is used (check the reviews on Amazon etc) from a reputable source. Make sure it can supply perhaps 2A or more (the Pi and display may consume this much).

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • vinceverc
    0 vinceverc over 9 years ago in reply to shabaz

    Thanks for the answer shabaz.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vinceverc
    0 vinceverc over 9 years ago in reply to shabaz

    I was thinking about the things you said about the display, but I watched the video from the ben heck show where they build the raspberrry pi portable (https://www.youtube.com/watch?v=Ko7eNx0zAuI ), and they say they used the lcd display they used in the portable atari build(https://www.youtube.com/watch?v=21qZKo0f280 ) , I watched that video and found the same screen on amazon (it has the same dimensions and looks identical), and it is way cheaper than the 7" display with a touchscreen, because I am still on a budget of course. And on the video the display was pretty easy to read. So i think i am going with that. If you think i am wrong please correct me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 9 years ago in reply to vinceverc

    Hi Vincent,

     

    I think that's ok, it is really down to what resolution you're comfortable with. I just wasn't sure if that would be enough, but it could be fine as you say.

    If you can aim to find a 5V one, then you can power everything from the USB 5V supply.