Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum what battery do i need?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 1793 views
  • Users 0 members are here
  • nimh
  • portable pi
  • help
  • battery
  • raspeberrypi
  • question
Related

what battery do i need?

vinceverc
vinceverc over 9 years ago

So i want to buld a raspberry pi portable. I am new to electronics and have a question.

It has to have a built in display and i will probably just connect a keyboard to it to configure it.

And i would like to give it a tablet like shape and just connect a usb mouse (I would also like to make it this way so i do not need a keyboard when using it, because it is portable and the mini keyboards cost a lot)

I found a backup display on amazon wich is 7 inches and needs 12v and 5 Wats

The raspberry pi needs 5 volts at 2.5 amps

So my question is: what battery do i need?

I watched a video about the types and i am going with a NiMH battery because the video said it was safe.

But what kind of ratings do i need?

Do i need a 17v battery and put the screen and pi in series, or do i fry something then?

And how di charge it? do i have to take out the battery when charging or can i connect the pi and screen to the charging circuit or something?

please help and sorry for this stupid question.

  • Sign in to reply
  • Cancel
Parents
  • the-dubster
    0 the-dubster over 9 years ago

    I'm not going to directly tell you which battery to use - but I AM going to say DO NOT put the screen and Pi in series - you'll kill the Pi or possibly them both!

     

    The same battery CAN supply both power requirements - just use regulators to give the 5V supply (The 12V can come directly from a 12V battery).

     

    If you use a higher voltage battery (14.4V for example) then a 12V Reg and a 5V reg will do the trick nicely.

     

    For regulators I often fall back on the 78XX series of 3 leg regulators (7805 for 5V and 7812 for 12V), depending on the power requirements will determine which style you need.

     

    Here are some links for the regs.

     

    Higher current devices are available and a heatsink will be required for full load.

     

    TAIWAN SEMICONDUCTOR - TS7805CZ - IC, V REG +5.0V, 7805, TO-220-3 | CPC UK http://cpc.farnell.com/taiwan-semiconductor/ts7805cz/ic-v-reg-5-0v-7805-to-220-3/dp/SC10582

     

    STMICROELECTRONICS - L7812CV - V REG +12V, 7812, TO-220-3 | CPC UK

     

    2A variant of the 5V

    STMICROELECTRONICS - L78S05CV - 5V, 2A Positive Voltage Regulator in TO-220-3 Package | CPC UK

     

    Also this is an option - the 7" touchscreen for the Pi - no need for 12V then as the included board takes care of the supply for you!

    Raspberry Pi 7” Touchscreen Display

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • vinceverc
    0 vinceverc over 9 years ago in reply to the-dubster

    Thanks for the quick answer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vinceverc
    0 vinceverc over 9 years ago in reply to the-dubster

    Thanks for the quick answer.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • the-dubster
    0 the-dubster over 9 years ago in reply to vinceverc

    No problems - shabaz mentions the same 7" Pi display in his reply - so 5V voltage requirements across the board makes life so much easier.

     

    The temptation to make (possibly) cheaper displays work can sometimes work out more expensive, more complex and less successful in the long run.