Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspbian 'PIXEL'  license agreement, Do you use it, have you read it? Are you concerned? (You should be)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 709 subscribers
  • Views 2290 views
  • Users 0 members are here
Related

Raspbian 'PIXEL'  license agreement, Do you use it, have you read it? Are you concerned? (You should be)

rive
rive over 9 years ago

What good an open source software distribution that you can't legally redistribute because it has proprietary parts?

The whole advantage of free and open source is that I can just fire up as many copies of the operating system as I like, give it to friends, slice and dice it - and never worry!

"Redistributing" is very general. If I made an RPi disk image and handed it to a friend, this is certainly "redistributing".

 

This isn't like "all commercial rights reserved" which we all understand is reasonable.

 

A regular user opens themself up to be sued for perceived damages, if they so much as post a screenshot of their 'PIXEL' desktop. or if it is determined they so much as crop or edit the image(s), or resizes it to any size other than "long edge at 1920px".

 

You cannot use the desktop images if you are a commercial entity (because if you are selling/including Raspbian PIXEL in, or with your Pi product, you violate the PIXEL licensing terms).

 

You cannot redistribute them period, for any reason, commercial or not. You ( the end user) do not own them, you cannot do with them as you please or even share them (e.g, 'redistribution'), and (you the end user) cannot even use them yourself on your system/Pi/hardware after 10 years, (at which time you are no longer covered under the use license, and you must remove them if they are installed).

 

If you violate the use/licensing terms, you can be sued for significant damages. You indemnify the rights holder/owner/representative agent/authorized third party against any and all claims (in other words, if you get sued for unauthorized use of the images, you cannot counter-sue for monetary loss, attorney's fees, defamation, etc).

 

 

Source: /usr/share/pixel-wallpaper

 

license.txt

 

The photographer grants the Licensee the non-exclusive, non-transferable and non-

assignable use of all images named above for 10 years, for the purpose of use as the

default wallpaper included within the Raspbian operating system, distributed by the

Raspberry Pi Foundation. The licence is “digital only” and for medium resolution

(long edge at 1920px), images shall not be used in any other form (such as in print

publications) nor for any commercial activities. However, use of the images to promote

the operating system and the activities of the Foundation (such as on social media, on

blogs and printed at trade shows) is acceptable.

 

Provisions:

The photographer retains all copyrights attached to the images as well as any other

rights which may not be detailed in this agreement.

 

Selling and/or redistribution of the images is forbidden.

 

Licensee is allowed to crop and/or electronically alter images to suit their purposes

for the usage stated above.

 

Indemnity:

The Licensee indemnifies and holds harmless Greg Annandale against all claims,

liability, damages, costs and expenses stemming from a breach of this agreement,

the use of the images, your failure to abide by any restriction regarding the use

of an image, or any claim by a third party related to the use of the images.

Attachments:
license.txt.zip
  • Sign in to reply
  • Cancel
Parents
  • gdstew
    0 gdstew over 9 years ago

    I have no idea what you are raving about. The license you are so worried about only applies to 16 images used for wallpaper in PIXEL for the photographer

    that supplied them. He is completely within his rights to spell out the copyright terms and conditions for the use of his images and I don't really have any

    problems with the terms he listed. If you don't like them, don't use any of his pictures for wallpaper and/or don't use them in any way that violates his

    terms (Michael).

     

    @ Michael

     

    "Nothing new here - the RPI Foundation has never given a damn about open source in the way that most of us understand it."

     

    This license isn't about open source code it's about photographs.

    Yes, it's not like you can get the source code for Raspbian and build it yourself, oh wait !

    Or like they have the ONLY fully documented GPU used in any ARM SOC, oh wait !

    Now if they would just publish their schematics I would be much happier with them.

     

     

    "It does serve to illustrate how incredibly careful you need to be when distributing a commercial product based on 'open source' code."

     

    You still need to be careful with distributing open source code in commercial products even if it does not include copyrighted photographs.

     

     

    "I want to know if Greg Annandale created the views he photographed, if he takes a picture with a bit of my garden in it can I assert my rights on that"

     

    Possibly, and if you could you would, like him, be completely within your rights to do so in any lawful terms you see fit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to gdstew

    The point that concerns me about this, and similar, bundling of copyright or otherwise restricted or protected material into a package that might reasonably be expected to be freely used is that it requires anyone who uses the bundle, for pretty much any purpose other than playing at home, to consider and understand the legal niceties of the terms.

     

    When the terms are one of the well known standard open source licenses there is a publicly available discussion, and even consensus as to their meaning - for the pictures this is not the case - I'm not a lawyer and I have no idea at all what the conditions mean and who they might apply to.

     

    BTW - if I finish a sentence with a image it generally means that I'm being ironic or attempting a joke - however not all jokes (or irony) are guaranteed to be so indicated.

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to gdstew

    The point that concerns me about this, and similar, bundling of copyright or otherwise restricted or protected material into a package that might reasonably be expected to be freely used is that it requires anyone who uses the bundle, for pretty much any purpose other than playing at home, to consider and understand the legal niceties of the terms.

     

    When the terms are one of the well known standard open source licenses there is a publicly available discussion, and even consensus as to their meaning - for the pictures this is not the case - I'm not a lawyer and I have no idea at all what the conditions mean and who they might apply to.

     

    BTW - if I finish a sentence with a image it generally means that I'm being ironic or attempting a joke - however not all jokes (or irony) are guaranteed to be so indicated.

     

    MK