Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Installing Code for PiFace Real Time Clock
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 52 replies
  • Answers 4 answers
  • Subscribers 708 subscribers
  • Views 8064 views
  • Users 0 members are here
  • raspberry_pi
Related

Installing Code for PiFace Real Time Clock

fc-element
fc-element over 9 years ago

Dear Element 14 Community.

All my Raspberry Pi devices (RPi 2, RPi Zero, and RPi 3 (planned) are running with the current Raspbian Jessie version. I have successfully installed PiFace Real Time Clock using the PiFace website instructions and GitHub.com software download on a number of RPi 2's and one of my three RPi Zero's.

 

I have recently continued the installations on another two RPi's and cannot continue because after these two lines:

1. chmod +x install-piface-real-time-clock.sh

2. sudo ./install-piface-real-time-clock.sh

 

The following new comments are returned: 1

1.. create new pifacertc init script to load time from PiFace RTC

2. Adding /etc/init.d/pifacertc .

3. install the pifacertc init script

4. enable I2c by using raspi-config

 

As I am a Linux beginner, can someone lead me through (expand) the coding of these lines so I may install PiFace RTC currently and in the future. The changelog on GitHub refers to a revision change but I am not knowledgable enough to understand why the install went through previously by not currently.

 

Thank you very much,

Frank.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Please note that the /etc/init.d folder is for the use of system service platforms like Upstart and Systemd (latest).  I would not put a script there.  If you want some low-level service to automatically start during the Linux boot process, the file /etc/rc.local is a better place to do this (somewhere before the `exit` command that is delivered in the installed rc.local).  On the other hand,  I cannot see the "GitHub.com software" you are talking about because you didn't mention the URL.  Please publish this.

     

    This one?

    https://github.com/jhowie/FreeBSDPiFaceRTC

     

    That one states to put the start up command in rc.local (good advice).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fc-element
    0 fc-element over 9 years ago in reply to e14 Contributor

    Dear texadactyl

    I just now saw your referral to another website I can try and I will do so in the net hour. I don't now if this will be successful. I've never seen this on the web and it appears that I'll have to learn- not knowing what BSD means right now. I'd appreciate your comment about using this method instead of the one descibed below.

    But as to your comment " I cannot see the "GitHub.com software" you are talking about, here is the following:

    Starting Website to Add PiFace Real Time Clock
    http://www.piface.org.uk/products/piface_clock/

    Two Links (located towards bottom of site) were followed:

    1. Documentation (downloaded pdf File)

    2. PiFace Real Time Clock on GitHub
    https://github.com/piface/PiFace-Real-Time-Clock

    Restating the issue
    Previous installations of PiFace RTC on both RPi 2 and RPi Zero following the procedure listed above have worked successfully.

    Currently, during the installation of additional RPi Zero devices. I ran into a problem which prevented me to continue.
    After the command:

    chmod +x install-piface-real-time-clock.sh 

    no problem was rncountered. However after I added:

    sudo ./install-piface-real-time-clock.sh

    The following four lines were returned:

    create new pifacertc init script to load time from PiFace RTC
    Adding /etc/init.d/pifacertc .
    install the pifacertc init script
    enable I2c by using raspi-config
    (and also suggestions as how to inable I2C.

    Within https://github.com/piface/PiFace-Real-Time-Clock, the changemod lists two versions (revisions): v0.2.0 which involves /etc/init.d/pifacertc script and v0.1.0 which involves the /etc/rc.local script. I thoroughly agree that rc.local is the best "option" since this is the path that worked in the past (I guess).

    As I am a Linux beginner, is there any method to select or "grab" the first version or,  solving the present issue, can someone give me the line-by-line coding of the first two lines which involve the script creation so I may install PiFace RTC in the future. This is the one you have not recommended.

    Ill be glad to explain further if there still is a miscommunication on my part.
    Frank.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fc-element
    0 fc-element over 9 years ago in reply to e14 Contributor

    Dear texadactyl

    I just now saw your referral to another website I can try and I will do so in the net hour. I don't now if this will be successful. I've never seen this on the web and it appears that I'll have to learn- not knowing what BSD means right now. I'd appreciate your comment about using this method instead of the one descibed below.

    But as to your comment " I cannot see the "GitHub.com software" you are talking about, here is the following:

    Starting Website to Add PiFace Real Time Clock
    http://www.piface.org.uk/products/piface_clock/

    Two Links (located towards bottom of site) were followed:

    1. Documentation (downloaded pdf File)

    2. PiFace Real Time Clock on GitHub
    https://github.com/piface/PiFace-Real-Time-Clock

    Restating the issue
    Previous installations of PiFace RTC on both RPi 2 and RPi Zero following the procedure listed above have worked successfully.

    Currently, during the installation of additional RPi Zero devices. I ran into a problem which prevented me to continue.
    After the command:

    chmod +x install-piface-real-time-clock.sh 

    no problem was rncountered. However after I added:

    sudo ./install-piface-real-time-clock.sh

    The following four lines were returned:

    create new pifacertc init script to load time from PiFace RTC
    Adding /etc/init.d/pifacertc .
    install the pifacertc init script
    enable I2c by using raspi-config
    (and also suggestions as how to inable I2C.

    Within https://github.com/piface/PiFace-Real-Time-Clock, the changemod lists two versions (revisions): v0.2.0 which involves /etc/init.d/pifacertc script and v0.1.0 which involves the /etc/rc.local script. I thoroughly agree that rc.local is the best "option" since this is the path that worked in the past (I guess).

    As I am a Linux beginner, is there any method to select or "grab" the first version or,  solving the present issue, can someone give me the line-by-line coding of the first two lines which involve the script creation so I may install PiFace RTC in the future. This is the one you have not recommended.

    Ill be glad to explain further if there still is a miscommunication on my part.
    Frank.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to fc-element

    I didn't mean that using an /etc/init.d/x script was invalid; it just runs the risk of becoming inoperative in the future if the service manager changes.  That is why user-level applications should avoid infrastructure folders unless they are willing to provide a methodology and documentation for each service manager in use by Unix and Linux.  I have done this too so I am no angel.  image

     

    "BSD" usually refers to University of California at Berkeley Unix as late as the 1980s, a precursor to Linux and MacOSX (based on BSD 4.4).

     

    Okay, I have seen the script.  It looks clearly written and very modular although it only provides a service start function (no stop or reload).  I'll stop being picky. 

     

    Having tried it myself, I just found out that this script is dependent on the OS being Raspbian.  Since I am currently running Ubuntu MATE on my Raspberry Pi, I could not go further.  It fails for me when it correctly diagnoses that the raspi-config service is missing.  I'll get out of the way and let you get help from folks who are using Raspbian.  Sorry that I couldn't be of more help.  If you have any general Linux questions, I can help you with that.  Maybe, I'll go back to Raspbian when I have a chance in the future.