Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Installing Code for PiFace Real Time Clock
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 52 replies
  • Answers 4 answers
  • Subscribers 708 subscribers
  • Views 8074 views
  • Users 0 members are here
  • raspberry_pi
Related

Installing Code for PiFace Real Time Clock

fc-element
fc-element over 9 years ago

Dear Element 14 Community.

All my Raspberry Pi devices (RPi 2, RPi Zero, and RPi 3 (planned) are running with the current Raspbian Jessie version. I have successfully installed PiFace Real Time Clock using the PiFace website instructions and GitHub.com software download on a number of RPi 2's and one of my three RPi Zero's.

 

I have recently continued the installations on another two RPi's and cannot continue because after these two lines:

1. chmod +x install-piface-real-time-clock.sh

2. sudo ./install-piface-real-time-clock.sh

 

The following new comments are returned: 1

1.. create new pifacertc init script to load time from PiFace RTC

2. Adding /etc/init.d/pifacertc .

3. install the pifacertc init script

4. enable I2c by using raspi-config

 

As I am a Linux beginner, can someone lead me through (expand) the coding of these lines so I may install PiFace RTC currently and in the future. The changelog on GitHub refers to a revision change but I am not knowledgable enough to understand why the install went through previously by not currently.

 

Thank you very much,

Frank.

  • Sign in to reply
  • Cancel
Parents
  • fc-element
    0 fc-element over 9 years ago

    Dear Ms tozer,

    Thanks for your speedy comments and otherwise approaches I had no knowledge of.

    No- I did not check these commands but I will do so in the near future. If in fact the installation was successfull, I still am getting a Failed line: Failed to Add PiFace RTC  during the boot phase but this may have been resolved within the remaining lines. To be honest when I have a returned response that I must create another init pifacertc script, I may not have proceeded successfully with the date verification and i2c-dev checking.  I'll continue to eperiment and thanks or you help. Frank.

    Dear Clem Martins,

    Thanks or your continuing interest.
    Yes- I swapped SD cards and BOTH RPi Zero systems failed. The SD cards are identical in brand, model, and capacity. However, I certainly may have proceeded slightly different in their installations. I should mention that installed on each system are also a WiPi network adapter, a Flash drive, and an ENC28j60 Ethernet module on a poered hub but all these components are performing admirably.

    In the future, I may recode Failed SD card from the beginning and install all the components rom scratch again. I would appreciate if you can recommend a specific Rasbpian Jessie version and also comment on the initial commands other than:   

    sudo apt-get update
    sudo apt-get upgrade

    In addition, there are a multitude of additional "switches" like,  sudo apt-get upgrade -y
    What are the current standards that I should use ?

    I also plan on cloning the successfull SD card on my windows laptop using notepad ++ and also examining each and every file to determine the differences from the failed SD card. You are certainly correct that something is different with these cards.

    Dear Sir, I promise I won't continue bothering you and Ms tozer with these seemingly simple problems
    Thans or your consideration.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • fc-element
    0 fc-element over 9 years ago

    Dear Ms tozer,

    Thanks for your speedy comments and otherwise approaches I had no knowledge of.

    No- I did not check these commands but I will do so in the near future. If in fact the installation was successfull, I still am getting a Failed line: Failed to Add PiFace RTC  during the boot phase but this may have been resolved within the remaining lines. To be honest when I have a returned response that I must create another init pifacertc script, I may not have proceeded successfully with the date verification and i2c-dev checking.  I'll continue to eperiment and thanks or you help. Frank.

    Dear Clem Martins,

    Thanks or your continuing interest.
    Yes- I swapped SD cards and BOTH RPi Zero systems failed. The SD cards are identical in brand, model, and capacity. However, I certainly may have proceeded slightly different in their installations. I should mention that installed on each system are also a WiPi network adapter, a Flash drive, and an ENC28j60 Ethernet module on a poered hub but all these components are performing admirably.

    In the future, I may recode Failed SD card from the beginning and install all the components rom scratch again. I would appreciate if you can recommend a specific Rasbpian Jessie version and also comment on the initial commands other than:   

    sudo apt-get update
    sudo apt-get upgrade

    In addition, there are a multitude of additional "switches" like,  sudo apt-get upgrade -y
    What are the current standards that I should use ?

    I also plan on cloning the successfull SD card on my windows laptop using notepad ++ and also examining each and every file to determine the differences from the failed SD card. You are certainly correct that something is different with these cards.

    Dear Sir, I promise I won't continue bothering you and Ms tozer with these seemingly simple problems
    Thans or your consideration.