Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Chipkit PI pin 8 and 9 not working?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 704 subscribers
  • Views 759 views
  • Users 0 members are here
  • pin 8
  • raspberry_pi
  • chipkit_pi
  • raspeberry_pi_accessories
  • arduino
  • pin 9
Related

Chipkit PI pin 8 and 9 not working?

e14 Contributor
e14 Contributor over 9 years ago

So I am trying to blink a couple of leds on pins 8 and 9, and not getting anything to work.

I've tried different pins, and the leds work, so I know it's not the leds.  I also tried different leds on pin 8 and 9 and nothing.

 

here is a snip of the code:

 

void setup() {

     pinMode(8, OUTPUT);

     pinMode(9, OUTPUT);

}

 

void loop() {

     digitalWrite(8, HIGH);

     delay(1000);

     digitalWrite(8, LOW);

     delay(1000);

     digitalWrite(9, HIGH);

     delay(1000);

     digitalWrite(9, LOW);

     delay(1000);

}

 

I'm not sure, but wondering if  a jumper needs to be set, I've search the net, and couldn't find an answer.  I did try to change the pin numbers to the PIC numbers and not the arduino numbers, still nothing.

 

Any one got any ideas what to try?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Looking at the pin relationships in the quick start guide, pins 8 & 9 are used for d+/d- (which are usually symbollic for usb data lines) so either they are reserved just for that function or you would have to find some way to alter the pin functions before you can use them as gpio pins. Im not familiar with the language or command set the chipkit pi uses so with going further into the documentation, this is all the help I can give right now but i hope it sheds some light on your issues and sets you on a path to resolve them. I used to do a lot of work with PIC's and in most cases it should be possible to change their function.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    Looking at the pin relationships in the quick start guide, pins 8 & 9 are used for d+/d- (which are usually symbollic for usb data lines) so either they are reserved just for that function or you would have to find some way to alter the pin functions before you can use them as gpio pins. Im not familiar with the language or command set the chipkit pi uses so with going further into the documentation, this is all the help I can give right now but i hope it sheds some light on your issues and sets you on a path to resolve them. I used to do a lot of work with PIC's and in most cases it should be possible to change their function.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to e14 Contributor

    Thank you,

    There are 2 jumpers marked D+ and D- on the board, I moved the jumpers and Pin 8 and 9 both work, I've been looking for a document that tells what all the jumpers do, but so far I have just found the quick start guides.  But I'll keep looking, I'm sure the information is somewhere on the net.

     

    Thanks again.