Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How to break out of a while True: loop with a button
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 706 subscribers
  • Views 12148 views
  • Users 0 members are here
  • raspberry_pi
Related

How to break out of a while True: loop with a button

flypadre
flypadre over 9 years ago

I've been working on some python scripts accessing the gpio pins on my rpi to light an led and I ran into a little problem I'm not sure how to solve.

My code looks something like this minus some setup statements

 

def ledblink():

     while True:

          GPIO.output(13, True)

          time.sleep(.5)

          GPIO.output(13, False)

          time.sleep(.5)

 

def ledoff():

     GPIO.output(13, False)

 

button = Button(root, text = 'LED ON', command = ledblink)

button.pack()

offbutton = Button(root, text = 'LED OFF', command = ledoff)

offbutton.pack()

 

As you can probably tell using tkinter for my gui. Also, as you can probably tell once I click the on button, that is all this program is going to let me do, the led blinks and continues because True is always True. How can I keep an indefinite loop running so that I can have a blinking led and still be able to break out of the loop when I want to turn things off? This was easy when I wanted to simply turn the led on and off, but not so easy with the loop I have to make it blink.

Just an FYI I was able to break out of the loop in my script version by using a try/except in which I used KeyboardInterrupt to call GPIO.cleanup() but I'm not sure how to do this in a gui.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • flypadre
    0 flypadre over 9 years ago

    OK This is what I thought I was being asked to do with regards to coding this without using threads, but this does not work either.

    import tkinter as tk
    import time
    
    root = tk.Tk()
    switch = False
    
    def blink(switch):
        while switch == True:
            print('BLINK...BLINK...')
            time.sleep(0.5)
        while switch == False:
            break
    
    def switchon():
        switch = True
        blink(switch)
    
    def switchoff():
        switch = False
        blink(switch)
    
    def kill():
        root.destroy()
    
    onbutton = tk.Button(root, text = "Blink ON", command = switchon)
    onbutton.pack()
    offbutton =  tk.Button(root, text = "Blink OFF", command = switchoff)
    offbutton.pack()
    killbutton = tk.Button(root, text = "EXIT", command = kill)
    killbutton.pack()
    
    root.mainloop()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to flypadre

    Sean,

    The "use threads" suggestion was a "future improvement" because it "might improve the performance". I tried to say that "improving performance" at this stage is NOT a good idea for two reasons. 1) I don't think it actually improves performance and 2) is detracts from the issue of trying to get things to work.

     

    I am not very familiar with the language you're using. But the way you've written the blink function is never going to work.

     

    You are calling the blink function, with either a true or a false argument. In the first case (true) the while switch==true will ALLWAYS be true and remain true, so the loop can never end. In the second case (false), when you call the function the while loop will simply never execute and the second while loop will issue a useless "break" function.

     

    IF you get threads to work, and IF they work in python the way they work in C, then....

    [code]

    def blink:

        while True:

             if (switch) print ('blink')

             time.sleep (0.5)

    [/code]

    Now YOU have to figure out how to make this a thread. (I googled this for you and it is too complicated for me to understand in 5 minutes).  This function will continue to run, even when switch is false, but then it won't do the blink. 

     

    You may have to do some python magic to make the "switch" variable a global variable.

     

    Now when your program starts you do create_thread (blink) (however that is written in python). When the "start blinking" button is pressed you simply set switch=True, and when stop blinking button is pressed you simply do switch=False;

     

    When "quit" is pressed you'd better somehow "kill" the thread that does the blinking.

     

    Another way to implement this is to simply CREATE the thread doing the blinking when the start button is pressed and to stop the thread when either the stop or quit button is pressed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to rew

    That code doesn't work very well for a responsive interface, you would need to be holding the button down throughout the sleep cycle in order for it to be tested when the if statement comes back around (for how long depends on when in the sleep cycle you started pressing the button. The worst case scenario would be pressing it for 0.5s which is a lot longer than anybody would like out of an on screen button. Also the light would only blink if the button was being held down). Not to mention that keeping the loop going when its not needed to blink the button is wholly inefficient and im sure you can agree that is just plain bad practice.

     

    The code I provided above is a direct drag and drop replacement for the original that doesnt use threading, im not going to say its the most efficient but it is working code that I tested before I posted and easy to read (for the sake of argument the performance increase of threading comes from not locking up a linux process and allowing it to be free'd up to do something else during the python threads sleep time, like draw the button to the screen efficiently, handle its file system, draw the desktop, send/recieve network data. All things that would benefit, when I talk about these things Im looking from an overall system advantage not just a narrow view of a single python script)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to rew

    That code doesn't work very well for a responsive interface, you would need to be holding the button down throughout the sleep cycle in order for it to be tested when the if statement comes back around (for how long depends on when in the sleep cycle you started pressing the button. The worst case scenario would be pressing it for 0.5s which is a lot longer than anybody would like out of an on screen button. Also the light would only blink if the button was being held down). Not to mention that keeping the loop going when its not needed to blink the button is wholly inefficient and im sure you can agree that is just plain bad practice.

     

    The code I provided above is a direct drag and drop replacement for the original that doesnt use threading, im not going to say its the most efficient but it is working code that I tested before I posted and easy to read (for the sake of argument the performance increase of threading comes from not locking up a linux process and allowing it to be free'd up to do something else during the python threads sleep time, like draw the button to the screen efficiently, handle its file system, draw the desktop, send/recieve network data. All things that would benefit, when I talk about these things Im looking from an overall system advantage not just a narrow view of a single python script)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • flypadre
    0 flypadre over 9 years ago in reply to e14 Contributor

    I tried to use the code that you supplied but I was unable to get it to work. Like before the interface locks up once the while loop was entered. image