Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum How to break out of a while True: loop with a button
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 22 replies
  • Subscribers 706 subscribers
  • Views 12148 views
  • Users 0 members are here
  • raspberry_pi
Related

How to break out of a while True: loop with a button

flypadre
flypadre over 9 years ago

I've been working on some python scripts accessing the gpio pins on my rpi to light an led and I ran into a little problem I'm not sure how to solve.

My code looks something like this minus some setup statements

 

def ledblink():

     while True:

          GPIO.output(13, True)

          time.sleep(.5)

          GPIO.output(13, False)

          time.sleep(.5)

 

def ledoff():

     GPIO.output(13, False)

 

button = Button(root, text = 'LED ON', command = ledblink)

button.pack()

offbutton = Button(root, text = 'LED OFF', command = ledoff)

offbutton.pack()

 

As you can probably tell using tkinter for my gui. Also, as you can probably tell once I click the on button, that is all this program is going to let me do, the led blinks and continues because True is always True. How can I keep an indefinite loop running so that I can have a blinking led and still be able to break out of the loop when I want to turn things off? This was easy when I wanted to simply turn the led on and off, but not so easy with the loop I have to make it blink.

Just an FYI I was able to break out of the loop in my script version by using a try/except in which I used KeyboardInterrupt to call GPIO.cleanup() but I'm not sure how to do this in a gui.

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • flypadre
    0 flypadre over 9 years ago

    OK This is what I thought I was being asked to do with regards to coding this without using threads, but this does not work either.

    import tkinter as tk
    import time
    
    root = tk.Tk()
    switch = False
    
    def blink(switch):
        while switch == True:
            print('BLINK...BLINK...')
            time.sleep(0.5)
        while switch == False:
            break
    
    def switchon():
        switch = True
        blink(switch)
    
    def switchoff():
        switch = False
        blink(switch)
    
    def kill():
        root.destroy()
    
    onbutton = tk.Button(root, text = "Blink ON", command = switchon)
    onbutton.pack()
    offbutton =  tk.Button(root, text = "Blink OFF", command = switchoff)
    offbutton.pack()
    killbutton = tk.Button(root, text = "EXIT", command = kill)
    killbutton.pack()
    
    root.mainloop()

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to flypadre

    My original test program also had the tkinter buttons in a thread so they were working independently. There is a very good chance that without using a thread at least once you will never be able to break out of the while loop in a responsive manner. Would you mind if I provided an example using threads? its really just going to be about 4 extra lines, with one of them being the import threads statement and is easy to understand. It would make your task so much simpler.

     

    For a responsive buttons without any threading you are going to have to add a for loop which contains a sleep function for a miniscule amount of time and a call to yield within the loop, then another master loop to control it all. Without using threads the code is going to need about 20 more lines to achieve this task

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to flypadre

    My original test program also had the tkinter buttons in a thread so they were working independently. There is a very good chance that without using a thread at least once you will never be able to break out of the while loop in a responsive manner. Would you mind if I provided an example using threads? its really just going to be about 4 extra lines, with one of them being the import threads statement and is easy to understand. It would make your task so much simpler.

     

    For a responsive buttons without any threading you are going to have to add a for loop which contains a sleep function for a miniscule amount of time and a call to yield within the loop, then another master loop to control it all. Without using threads the code is going to need about 20 more lines to achieve this task