Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Pi 3 board failure?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 4072 views
  • Users 0 members are here
  • power supply
  • raspberry_pi
  • rasberry pi 3
Related

Pi 3 board failure?

sunnydale102
sunnydale102 over 9 years ago

I recently received a Pi 3 B. I've installed jessie and I've been running it without issues for a couple of weeks.

 

Last week I turned on the power and waited for the console output and saw nothing.

 

The red LED on the power supply monitor flashes, which I believe indicates that the power supply is low. After about 60 seconds or so of flashing the LED goes out. There is also some flashing on the green LED during this time.

 

I've probed PP35 on the 5V input and noted that the supply is indeed low, about 4.5, and declines until it drops below 3.5V at which point the red LED goes out. I've tried various alternate USB power supplies and all show identical results. No smoke, nothing feels unusually warm so there's no obvious fault.

 

Note that both the power supply and the SD card work as expected on my test Pi 1 B. I realize that the Pi 1 draws less current but it all worked fine for a couple of weeks.

 

Any suggestions?

 

Thanks

 

"Sunny"

  • Sign in to reply
  • Cancel
Parents
  • sunnydale102
    0 sunnydale102 over 9 years ago

    After some further investigation I've done a bit of testing and here's the test and results:

    As noted in my original post I was running the Pi3 without incident one day and turned it on the next and it refused to boot.

    The symptoms; flashing red LED and flashing green LED for about 20 - 30 seconds then both red and green LEDs go out. Periodically after that the green LED will flash sporadically.

     

    My test.

    I suspected something in the 5V input failed so I bypassed the PTC, and MOSFET and applied power to the 5V pins on the header.

    The power is from an Adafruit bread board power supply so it is limited to about an amp. I monitor both the 5V rail and a 3.3V pin on the header.

    I monitor the console output on the TX pins with a Pi USB serial again from Adafruit.

     

    Results:

    With the above arrangement I see a steady red LED and flashing green LED. Both the 5V and 3.3V rails are steady and at the correct voltage.

    There is no output on the console so I retried with my network connected and ping just in case there's something wonky with the serial I/O.

    Nothing feels hot to the touch on either side of the board.

     

    Note that the boot SD card, serial connector and network connection all work correctly when attached to my Pi1.

     

    I've resigned myself to the fact there's a component failure and I have a $80 brick ( that's the cost CDN for the board + delivery).

     

    Any other ideas would be most appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sunnydale102
    0 sunnydale102 over 9 years ago

    After some further investigation I've done a bit of testing and here's the test and results:

    As noted in my original post I was running the Pi3 without incident one day and turned it on the next and it refused to boot.

    The symptoms; flashing red LED and flashing green LED for about 20 - 30 seconds then both red and green LEDs go out. Periodically after that the green LED will flash sporadically.

     

    My test.

    I suspected something in the 5V input failed so I bypassed the PTC, and MOSFET and applied power to the 5V pins on the header.

    The power is from an Adafruit bread board power supply so it is limited to about an amp. I monitor both the 5V rail and a 3.3V pin on the header.

    I monitor the console output on the TX pins with a Pi USB serial again from Adafruit.

     

    Results:

    With the above arrangement I see a steady red LED and flashing green LED. Both the 5V and 3.3V rails are steady and at the correct voltage.

    There is no output on the console so I retried with my network connected and ping just in case there's something wonky with the serial I/O.

    Nothing feels hot to the touch on either side of the board.

     

    Note that the boot SD card, serial connector and network connection all work correctly when attached to my Pi1.

     

    I've resigned myself to the fact there's a component failure and I have a $80 brick ( that's the cost CDN for the board + delivery).

     

    Any other ideas would be most appreciated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • royleith
    0 royleith over 9 years ago in reply to sunnydale102

    When you said 5V on the header, did you mean the GPIO 5V pin?

     

    All of my Pis light their red LEDs for as long as power is supplied. For earlier models when I made a key mistake of using a poor-quality, powered USB hub, that was even the case when the main 5V power was cut, but the USB hub power was still connected (the hub was passing power back to the Pi, which is a real no-no).

     

    The fact that the green light flashes seems to show that something is being booted from the SDHC card and that the regulator is supplying 5V and 3.3v for at least part of the time. Your last test seems to indicate that the switching regulator is working well. I don't know why the red LED is flashing and not staying on, permanently, but the answer may be in the early boot serial output.

     

    I have never investigated the serial output from the early boot stages using the serial port, but my thought is that the moment an HDMI screen is detected, the OS is configured to route the serial output to that screen. The OS does a lot of auto-configuring during the first boot. Cards that boot well on some of my Pis cause a kernel panic on the Pi 3. I don't know what is required to divert the serial stream to the serial port, but I don't think it happens automatically when the monitor is disconnected. That might be the reason you're not seeing anything on the serial port.

     

    I think the blank HDMI monitor is another issue entirely and that needs to be resolved in order to see the serial stream.

     

    Sometimes all the Pis will have problems with HDMI monitors. My Pi 3 booted into low resolution instead of 1080p. Other folk get nothing at all because the Pi is outputting an HDMI signal that the monitor or TV cannot handle. I think you should revert to conventional power and HDMI and make sure that the HDMI monitor will be driven. I'm assuming a PAL 1080p 16:9 HDMI monitor. If you are using something else, you need to check,

     

    RPiconfig - eLinux.org

     

    Here are the lines in my config.txt which force HDMI boost and force PAL 1080p 16:9, HDMI resolution. I don't know if the sdtv settings are actually required, but, if it works...

     

     

    # uncomment to increase signal to HDMI, if you have interference, blanking, or

    # no display

    config_hdmi_boost=4

     

    # For 1080p display

    sdtv_mode=2

    sdtv_aspect=3

    hdmi_group=1

    hdmi_mode=16

     

    Note: sdtv_mode=0 switches to Normal NTSC.

     

    If you still don't get anything on the monitor, try the following,

     

    # uncomment if you get no picture on HDMI for a default "safe" mode

    hdmi_safe=1

     

    # uncomment if hdmi display is not detected and composite is being output

    hdmi_force_hotplug=1

     

    I have not found these lines to be helpful, but it depends on the screen.

     

    The early boot screen should give you some view of what is going wrong.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to royleith

    Roy Leith wrote:


    All of my Pis light their red LEDs for as long as power is supplied. For earlier models when I made a key mistake of using a poor-quality, powered USB hub, that was even the case when the main 5V power was cut, but the USB hub power was still connected (the hub was passing power back to the Pi, which is a real no-no).

    The passing back of power from the hub to the pi is said to be "bad" by a lot of people. But it's not that bad. It can lead to unexpected situations, that you think you make the pi powerless, but it remains running.

     

    Newer pi's have a circuit that is tuned to indicate "4.65V or more". This is then forwarded to the red led. So the red led on means: we have 4.65V or more and no red led means "4.64V or less".

     

    The fact that the green light flashes seems to show that something is being booted from the SDHC card and that the regulator is supplying 5V and 3.3v for at least part of the time. Your last test seems to indicate that the switching regulator is working well. I don't know why the red LED is flashing and not staying on, permanently, but the answer may be in the early boot serial output.

     

    "Flashing" can mean different things.  A regular flash is something entirely different from what we expect, a semi-random on-and-off with periods of "indistiguishable from on" and short periods of "off".

     

    I have never investigated the serial output from the early boot stages using the serial port, but my thought is that the moment an HDMI screen is detected, the OS is configured to route the serial output to that screen. The OS does a lot of auto-configuring during the first boot. Cards that boot well on some of my Pis cause a kernel panic on the Pi 3. I don't know what is required to divert the serial stream to the serial port, but I don't think it happens automatically when the monitor is disconnected. That might be the reason you're not seeing anything on the serial port.

     

    In principle, this is not autodetected, as far as I know. The kernel is normally booted with console=/dev/ttyAMA0 console=/dev/tty0  (or something equivalent on newer pi's.) So the (early) kernel output goes both ways.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 9 years ago in reply to rew

    Thanks Roger,

     

    My enduring feelings of guilt for using cheap powered USB hubs are assuaged.

     

    I am more convinced than ever that the Pi is working after a fashion.

     

    My suggestion, now, is to revert to standard connections with the changes to the config.txt settings to get HDMI working, but keep monitoring the serial port as well as the HDMI monitor. In addition, monitor the 5V rail closely during boot (which is relatively short) and see if it dips towards the 4.65V figure that Roger supplied. It seems unlikely as you are using a PSU delivering 5.1V or 5.2V. However, a switched mode PSU that has gone on the blink might drop its voltage during the higher current boot phase.

     

    You don't say how you are monitoring the TX port. I use putty on a Linux desktop or a second Pi and, in my experience, USB serial ports do not appear as /dev/tty0 or /dev/tty1 in the Pi, but more likely /dev/ttyusb0. You will have to hunt around for it in /dev (or your chosen computer equivalent) and set up putty to use that device. I noticed the following at RPi Serial Connection - eLinux.org

     

    • Built-in (standard) Serial Port: the Linux standard is /dev/ttyS0, /dev/ttyS1, and so on
    • USB Serial Port Adapter: /dev/ttyUSB0, /dev/ttyUSB1, and so on.
      • Some types of USB serial adapter may appear as /dev/ttyACM0

     

    NOTE FOR RASPBERRY PI 3: The Raspberry pi 3 has changed things a bit and you might need to add the option enable_uart=1 at the end of /boot/config.txt.

    Speed (baud rate): 115200

    • Bits: 8
    • Parity: None
    • Stop Bits: 1
    • Flow Control: None

    It would be a good move to make sure it is working with the TX pin of another Pi. There is no reason why the the console device has to be a Pi. It could, just as easily, be a Windows or other Linux computer. Both Windows and Linux support putty.

     

    And finally, if you can bear it, re-image the SDHC card and make the changes to config.txt before booting it.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • sunnydale102
    0 sunnydale102 over 9 years ago in reply to royleith

    Hi Roy,

    Your questions:

    "When you said 5V on the header, did you mean the GPIO 5V pin?"

    Yes. I've measured and it appears directly connected to the network on the schematic "5V" which is the protected bus at PP7. See the "Power In" portion of the schematic.

     

    "You don't say how you are monitoring the TX port"

    From my response above - "I monitor the console output on the TX pins with a Pi USB serial again from Adafruit."

    I connect to this with Putty with the appropriate parameters.

     

    Note from my original post, that this all worked fine when I turned things off. I'd been configuring the system and running for a couple of weeks before this happened.

     

    Also, as noted above, the only connections to the board are an network connector and the serial port cables (TX, RX, gnd, - no power from the USB) , other than power and ground from my bread board power supply of course. As I said originally, all this works fine on my Pi1.

     

    "And finally, if you can bear it, re-image the SDHC card"

    I've re-imaged the boot card and tested it on my Pi1 with jessie lite which is the "headless" version. It works just fine there. The Pi3 will boot another image of course but other than that, all else is identical.

    Note also that there is no network response to ping as there was when the board was functional.

     

    Kinda frustrating I know, but maybe this is a case of "infant mortality". My Pi1s ( I have two) have been working since I got them several years ago, one of which has run for hours a day without issue.

     

    Thanks for your interest and thoughts.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • royleith
    0 royleith over 9 years ago in reply to sunnydale102

    Hi Sunny,

     

    As I said

    The OS does a lot of auto-configuring during the first boot. Cards that boot well on some of my Pis cause a kernel panic on the Pi 3.

    The effect of the kernel panic on the Pi 3 is that the red LED comes on and the green LED flashes, but the OS does not complete booting. I propose reflashing, setting up config.txt and only booting on the Pi 3 to avoid mis-configuration. You do not say if you intend to run the Pi 3 in headless mode. If you do, you need to add the option enable_uart=1 at the end of /boot/config.txt in order to see the boot phase in putty and see what is going wrong.

     

    Booting in full fat Raspbian would provide both the console output and the 'Rainbow Square' low voltage warning that may not be properly indicated on a voltmeter (especially a digital one with its sampling delay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to royleith

    The rainbow-square as an indication for "not enough power" was replaced by a yellow powerbolt in a recent update.