Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rpi python problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 761 views
  • Users 0 members are here
Related

Rpi python problems

realringer
realringer over 9 years ago

Hi,

Im currently working on a raspberry pi zero timelapse project. The idea is to have a rpi zero with a cameramodule conected to it. Also conected is a wifi module wich takes up the one usb port. I want to avoid getting a usb hub.

 

I got a button connected which is runned by a program. when the button is pressed it runs my main program.

My main concists of a loop which takes a picture every few minutes and uploads it to my dropbox acc wia the wifi connection.

 

The problem lies in when i dont have a screen or are shh into the pi. I have done some reserch and figured out that the comand im using to upload to dropbox and deleating the image does not work without the shell. I have tried to fix this but havent figured it out jet. Is there an other option for uploading it and deleating the image. Im locking for a option that does not require a shell but still works fine with my code. its a python progam.

 

Thx in advance!!

Christofer.image

  • Sign in to reply
  • Cancel
Parents
  • urkraft
    0 urkraft over 9 years ago

    What about installing the screen utility on the raspi and changing the setup to boot into your program in a screen session. If you do not already have the screen utility installed you can install it with the following commands:

    sudo apt-get install screen

    sudo reboot

    In order to change your setup to boot into a screen session running your program enter the following line just before the “exit 0” line in the rc.local file which is located in the “/etc”  folder:

    su – pi –c “screen –dm –S pistartup /home/pi/python_code/Timelapse.py”

     

    This assumes that your python program is “Timelapse.py” and is located in the “/home/pi/python_code” folder. If your program is dependent on other things which also need to be launched first (like for example the pigpiod utility) then you will also need to enter lines for launching these in the rc.local file. For example the line for launching the pigpiod utility is:

    su –c “pigpiod”

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • urkraft
    0 urkraft over 9 years ago

    What about installing the screen utility on the raspi and changing the setup to boot into your program in a screen session. If you do not already have the screen utility installed you can install it with the following commands:

    sudo apt-get install screen

    sudo reboot

    In order to change your setup to boot into a screen session running your program enter the following line just before the “exit 0” line in the rc.local file which is located in the “/etc”  folder:

    su – pi –c “screen –dm –S pistartup /home/pi/python_code/Timelapse.py”

     

    This assumes that your python program is “Timelapse.py” and is located in the “/home/pi/python_code” folder. If your program is dependent on other things which also need to be launched first (like for example the pigpiod utility) then you will also need to enter lines for launching these in the rc.local file. For example the line for launching the pigpiod utility is:

    su –c “pigpiod”

     

    Good luck!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • realringer
    0 realringer over 9 years ago in reply to urkraft

    Thanks for the answer!

     

    It seams to be a sulution. However i cant test it untill later this week. My pi zero ip adress seams to have changed since i last logged in. Weird because i had a static ip setted up. When i connect the micro sd with the os to a different pi i got the new ip address. But when i tried to shh again i failed to get contact with the zero using the new ip. I deffinetly need a bit of thinking and trial and error. Im quite buissy this week so it has to wait.

    Thanks though, i will get right on it when i have the time.

     

    Christofer