Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Rpi python problems
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 707 subscribers
  • Views 756 views
  • Users 0 members are here
Related

Rpi python problems

realringer
realringer over 9 years ago

Hi,

Im currently working on a raspberry pi zero timelapse project. The idea is to have a rpi zero with a cameramodule conected to it. Also conected is a wifi module wich takes up the one usb port. I want to avoid getting a usb hub.

 

I got a button connected which is runned by a program. when the button is pressed it runs my main program.

My main concists of a loop which takes a picture every few minutes and uploads it to my dropbox acc wia the wifi connection.

 

The problem lies in when i dont have a screen or are shh into the pi. I have done some reserch and figured out that the comand im using to upload to dropbox and deleating the image does not work without the shell. I have tried to fix this but havent figured it out jet. Is there an other option for uploading it and deleating the image. Im locking for a option that does not require a shell but still works fine with my code. its a python progam.

 

Thx in advance!!

Christofer.image

  • Sign in to reply
  • Cancel
Parents
  • royleith
    0 royleith over 9 years ago

    I've always used the old os module. However, this link seems to have the answer,

     

    http://sharats.me/the-ever-useful-and-neat-subprocess-module.html

     

    You are using shell=true. It's used to get the enhanced features of the shell such as pipes. It does not look as though you are using shell features so use the shell=false mode.

     

    BTW the correct usage of shell=true is to use a string of the required shell command,

     

    call('ls -l', shell=True)

     

    It looks as though the syntax you are using is actually that of shell=false which requires a list of the program and arguments.

     

    call(['ls', '-l'])

     

    So, try

     

    call ([photofile])

    call ([photerm])

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • realringer
    0 realringer over 9 years ago in reply to royleith

    When i first encountered this problem i thought it had to do with the  shell=True . I therefore tried

    shell=False  aparently i was on the right track. But i didnt read the documentation and therefore it probebly were some faults. I got a errormessage when i tried it and moved on with other tries to fix it.

    Thanks for the link and im going to take a look at it when i get my rpi working again. I might just get my pi 3 and get the dropbox stuff sorted out tomorrow. Before i get into the ssh stuff and setting up the network again on the zero.

    Thanks again

     

    Christofer

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • realringer
    0 realringer over 9 years ago in reply to royleith

    When i first encountered this problem i thought it had to do with the  shell=True . I therefore tried

    shell=False  aparently i was on the right track. But i didnt read the documentation and therefore it probebly were some faults. I got a errormessage when i tried it and moved on with other tries to fix it.

    Thanks for the link and im going to take a look at it when i get my rpi working again. I might just get my pi 3 and get the dropbox stuff sorted out tomorrow. Before i get into the ssh stuff and setting up the network again on the zero.

    Thanks again

     

    Christofer