Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Line in to Line out: Poor sound quality
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 705 subscribers
  • Views 1025 views
  • Users 0 members are here
  • raspberry pi3
  • sound quality
Related

Line in to Line out: Poor sound quality

cpaulevans
cpaulevans over 9 years ago

Question: Am I missing some setting in getting best sound quality when playing line in to line out?

 

Background

 

I have the card on a Pi3 and following the various advice here and elsewhere I have got line in playing to line out. The purpose is to give me a volume control between line output from a DAC (Cambridge DacMagic 100) and input to a set of powered speakers.

 

When I connect the DAC to the speakers directly I get good sound quality. But the only volume control available is physically on touch buttons on one of the speakers. I assumed that one way to get a remote volume control was to use the card - probably eventually with Rune Audio or Volumio, For the moment I am using scripts and Alsamixer to do the set up and control. The volume is indeed controlled.

 

However the sound output is distinctly poor - best described as "muddy" - so it looks as though the processing through the card clips something out of the signal. Or maybe there is an electrical mismatch somewhere.

 

I plan to try two tests:

 

1: to record from the line in and then play the recording through line out. No real reason why this should improve things but it might show a difference.

2: to use a script that pipes the signal through an equaliser: no obvious reason why adding a stage would help but again worth a go.

 

However have spent a fair time having to read lots of posts to get the basics working I wonder whether I am missing something  obvious - hence my question. Very grateful in advance for any suggestions or pointers.

 

Paul

  • Sign in to reply
  • Cancel
  • cpaulevans
    0 cpaulevans over 9 years ago

    I have now belatedly seen this thread

    https://www.element14.com/community/message/199022/l/audio-passthrough-quality#199022

     

    which describes the same problem.

     

    I have found that this is an intermittent problem. There is no obvious correlation with anything of the settings. Most times a reboot comes back with good sound, sometimes there is a problem. I have now set up runeaudio to work as a volume control and set up the inputs and outputs using alsamixer rather than scripts

     

    My suspicion is that it is to do with the order of powering up the various components: TV, DAC, Cirrus but I have no evidence!!

     

    Paul