Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum can we use the raspberry pi 3 model b for the radioshack robotics starter kit
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 706 subscribers
  • Views 760 views
  • Users 0 members are here
  • raspberry_pi
Related

can we use the raspberry pi 3 model b for the radioshack robotics starter kit

brad2
brad2 over 9 years ago

can we use the raspberry pi 3 model b for the radioshack robotics starter kit instead of using the arduino uno

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 9 years ago

    No, the headers on the kit fit on an Arduino or compatible but not a Raspberry Pi 3. Also the Make:it motor driver board comes pre-programmed and you cannot upload any programs to this board. The programming at https://github.com/RadioShackCorp/2770168-MakeItRobotics-Starter-Kit is for an Arduino as well.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to clem57

    If you wan to go commando and go outside the box, http://www.joestechblog.com/category/robots/ has explained how the Arduino works with the motor control and sensors. With that he implies the Raspberry Pi could be used instead of the Arduino.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brad2
    0 brad2 over 9 years ago in reply to clem57

    i am trying to find where it talks about the raspberry pi but i an not find it

     

    Brad Harris

    (615) 974-8596

    bradley.harris002@gmail.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 9 years ago

    The simple answer is yes you can but with a couple of tasks before you will get it working

    1. The Arduino talks to the board using software serial on pins 2 and 3 and has level shifter circuit to adapt to 5V (The Dragon chip is 3V3 as is the PI), this level shifter will need to be bypassed to make it all work at 3V3. (A simple task with a soldering iron)

    2. You will need to study the arduino code to see the serial commands and responses used to talk to the board and re-code in python, C, C++ or whatever your programing language of choice is. There are a few LED outputs that can be connected to GPIO of the PI

    You won't be able to monitor the batter voltage as the PI has no ADC (You could add a separate one.

    The wiring will have to be via jumpers as the motor shield will not sit on the PI

     

    Reference is this https://github.com/RadioShackCorp/2770168-MakeItRobotics-Starter-Kit/blob/master/Schematics/2770168-CorePCB_schematic.pd…

    All the code is here for the arduino https://github.com/RadioShackCorp/2770168-MakeItRobotics-Starter-Kit/blob/master/Library/MakeItRobotics/MakeItRobotics.c…

    and it is easy to see how to talk to the board via a serial connection