Raspberry Pi
  • Products & Partners
  • More
Raspberry Pi
Raspberry Pi Forum When I purchase my raspberry PI 3, will I need a cooling fan to keep it cool as I plan to add a heat sync to the main chip?  Will I need a special case in which to mount a cooling fan?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 705 subscribers
  • Views 943 views
  • Users 0 members are here
  • raspberry_pi_space
Related

When I purchase my raspberry PI 3, will I need a cooling fan to keep it cool as I plan to add a heat sync to the main chip?  Will I need a special case in which to mount a cooling fan?

wrustylane
wrustylane over 9 years ago

When I finally purchase my Raspberry PI 3, will I need a cooling fan to keep it cool and I plan to add a heat sync to the main processor chip.  Will I need a special case to enclose the PI with a cooling fan?  If so, what would you suggest.  I'll probably get the Raspberry PI 3 with the camera module for a starter pack.  Any suggestions?  Also I would like to know if there is a micro camera that will interface with the PI 3 using WiFi as I plan to mount a camera in the nose of one of my HO scale engines for a look around the layout.  Any information would be greatly appreciated.  Thanks.  Rusty

  • Sign in to reply
  • Cancel
Parents
  • simpsonron
    0 simpsonron over 9 years ago

    My Pi 3 does not have a heat sync.  Just sitting on the desk not in a box.  On cold days (in doors) it is fine.  In the summer it will drop back in speed to keep the temperature under control.  1200_> to 600  It is on the edge of working at full speed with out heat syncs.  I will add a small heat sync.  If it was in a box with no air flow then it should have a fan.

     

    On the internet there are many small boxes, many with fan mounting holes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • wrustylane
    0 wrustylane over 9 years ago in reply to simpsonron

    Thank you very much for the information.  I will keep it in mind when (if ever) I'm able to buy a RPI3.  I've seen several different heat syncs shown in comments about cooling the RPI3.  I shall look for an enclosure that will not only house the RPI3, but will allow for installing a small fan for cooling.  Operating temperature need not be a variable with which I need to deal.  I'd rather add a cooling fan than loose speed on the main board due to temperature.  --Rusty

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • wrustylane
    0 wrustylane over 9 years ago in reply to simpsonron

    Thank you very much for the information.  I will keep it in mind when (if ever) I'm able to buy a RPI3.  I've seen several different heat syncs shown in comments about cooling the RPI3.  I shall look for an enclosure that will not only house the RPI3, but will allow for installing a small fan for cooling.  Operating temperature need not be a variable with which I need to deal.  I'd rather add a cooling fan than loose speed on the main board due to temperature.  --Rusty