Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum New Raspberry-Pi 3, Green-LED keeps blinking.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 707 subscribers
  • Views 11625 views
  • Users 0 members are here
  • raspberry_pi_space
Related

New Raspberry-Pi 3, Green-LED keeps blinking.

raife
raife over 9 years ago

I just received a Raspberry-Pi -3-B. The kit from "LoveRPI" (apparently, via Amazon.com) contained a Pi from "Element-14" and a no-name power-supply. I installed the latest "Raspian w/ Jessi" on a "SanDisk MicroSDHC UHS-I Class-10 16GB card", and discovered that the included power-supply was DOA (looked online, others have complained, a lot, about these Power-supplies). However, I have several other Pi models and switched to another 2.5A Micro-USB power-supply that I have. The Pi boots and everything seems to work, fine (blazingly-fast), networking, software, etc... However, when the Pi is doing nothing (with no software actively running, zero CPU-usage) the SD-Card-access-light (green LED) blinks continuously (about once a second). The Red-LED is steady. I have not noticed this on my other Raspberry-Pi's. Is this normal? Is this caused by my SD-Card? Is my Pi damaged (possibly by the original power-supply)?

 

Also... a silly question... my "Element14 Raspberry-Pi" (inside the "element14" box) came in a paper/cardboard envelope, instead of a regular anti-static bag. The envelope does have the "Element14" logo, so is this all OK? I'm a little nervous after the power-supply problem. Thanks.

  • Sign in to reply
  • Cancel
Parents
  • raife
    0 raife over 9 years ago

    Here is the latest. I discovered that the power-supply is actually a 2.0A (I have used it for some time on a Raspberry-Pi 2), and I have also tried another, new, 2.0A micro-usb power-supply, that I have. I have run the Raspberry-Pi-3 for several hours without any apparent issues. The only symptom (an, approximately, 1/3-second flash of the ACT-LED, about every second) continues whenever I am not actively interacting with the Pi. Otherwise, I would not even suspect anything was wrong at all. Does anyone know how to determine whether the flashing LED indicates actual SD-card access (OS logging, or some other internal OS operations, maybe?), or whether it is some kind of error-condition?

     

    As I stated earlier, this is a brand-new Raspberry-Pi 3B (my first Pi-3), with a fresh install of pure (not "noobs") "Raspbian-Jessie PIXEL". And, none of my other Pi's exhibit this type of continual LED/SD-card access-flashing (including my other "Raspbian-Jessie PIXEL" installations, on my Pi-2). So, is this just normal SD-card access, or is this unusual? How can I monitor actual SD-card RWs? I am suspecting, based upon the otherwise seemingly normal operation, that there is some actual storage-device operation going-on in the background. Can I (and should I) disable this repetitive storage device access? As I said, it just doesn't seem right that a Raspberry-Pi LED should continually be flashing (unlike the other Raspbian installations that I have). Perhaps, I should re-format the SD-card, and re-install "Raspbian-Jessie".

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to raife

    Hello Raife,

    AFAIK there is no direct relation between the led and the SD card access (I suppose to avoid any slowdown in the SD card reading).

    Anway, I suggest to read the very useful information specifically relate to the Raspberry PI Linux and hardware behaviour on the e-linux.org site. The behaviour of the green led is shown below, but I have not yet tested if this is coherent with the last hardware versions of the board (model 3B)

    the green light will blink in a specific pattern to indicate some types of errors:

    • 3 flashes: loader.bin not found
    • 4 flashes: loader.bin not launched
    • 5 flashes: start.elf not found
    • 6 flashes: start.elf not launched
    • 7 flashes: kernel.img not found

    Firmware since 20th October 2012 no longer requires loader.bin, and the flashes mean:

    • 3 flashes: start.elf not found
    • 4 flashes: start.elf not launched
    • 7 flashes: kernel.img not found
    • 8 flashes: SDRAM not recognised. You need newer bootcode.bin/start.elf firmware.

    If start.elf won't launch, it may be corrupt.

    Note that 4-flashes may point to a defective SD-card holder, if one or more of the data contacts is intermittent it can lead to this problem.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to raife

    Hello Raife,

    AFAIK there is no direct relation between the led and the SD card access (I suppose to avoid any slowdown in the SD card reading).

    Anway, I suggest to read the very useful information specifically relate to the Raspberry PI Linux and hardware behaviour on the e-linux.org site. The behaviour of the green led is shown below, but I have not yet tested if this is coherent with the last hardware versions of the board (model 3B)

    the green light will blink in a specific pattern to indicate some types of errors:

    • 3 flashes: loader.bin not found
    • 4 flashes: loader.bin not launched
    • 5 flashes: start.elf not found
    • 6 flashes: start.elf not launched
    • 7 flashes: kernel.img not found

    Firmware since 20th October 2012 no longer requires loader.bin, and the flashes mean:

    • 3 flashes: start.elf not found
    • 4 flashes: start.elf not launched
    • 7 flashes: kernel.img not found
    • 8 flashes: SDRAM not recognised. You need newer bootcode.bin/start.elf firmware.

    If start.elf won't launch, it may be corrupt.

    Note that 4-flashes may point to a defective SD-card holder, if one or more of the data contacts is intermittent it can lead to this problem.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer