Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry pi 3 GPIO not working
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 708 subscribers
  • Views 6957 views
  • Users 0 members are here
  • gpio
  • raspberry_pi
  • raspberry pi 3 gpio
Related

Raspberry pi 3 GPIO not working

byrd
byrd over 9 years ago

I am currently trying to turn an LED off but it is not working. (LED is always on, yes I do have a resistor 220 ohm)

 

I have Wiringpi installed and looking at the readall data I do not see any change when I run my commands.

 

I have tried directly in the python program, creating a python script and running it, running python from terminal, and using the wiringpi gpio commands. I have also tried doing all of this with sudo as well.

 

import RPi.GPIO as gpio
gpio.setmode(gpio.BCM)
gpio.setup(17, gpio.OUT)
gpio.output(17, False)

  • Sign in to reply
  • Cancel
Parents
  • royleith
    0 royleith over 9 years ago

    I have spent years collecting vital information about the various releases of the Pi to document the differences so that I can apply that to GPIO operations. It's about time I got on with actual bit bashing.

     

    I got this from the official raspberry GPIO Python site,

     

    https://sourceforge.net/p/raspberry-gpio-python/wiki/Examples/

     

    To specify which you are using (mandatory):

    GPIO.setmode(GPIO.BOARD)
      # or
    GPIO.setmode(GPIO.BCM)

    You are using the numbering of the GPIO pins on the BCM controller rather than the BOARD numbers of the Raspberry Pi GPIO. The following chart does not relate to all Pi revisions, but should be OK for the Pi 3.

    image

    So the BCM GPIO pin 17 (the one you are controlling) is actually Raspberry Pi GPIO pin 11. Could this be the problem? I notice that Pi pin 17 is a 3.3Volt pin which would light any LED via a resistor to Ground.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to royleith

    With the code setting the output LOW, I would hope the led is between 3.3V an the pin...

     

    To prevent this kind of mistake, you can try flashing the led: turn it on wait a while, turn it ff again. If you get the hardware polarity wrong, you can still see it flash...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rew
    0 rew over 9 years ago in reply to royleith

    With the code setting the output LOW, I would hope the led is between 3.3V an the pin...

     

    To prevent this kind of mistake, you can try flashing the led: turn it on wait a while, turn it ff again. If you get the hardware polarity wrong, you can still see it flash...