Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum RPi3 internet and receive calls
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 1432 views
  • Users 0 members are here
  • raspberrypi.
  • rpi3
  • raspberry pi
  • networking
  • usbmodem
Related

RPi3 internet and receive calls

matevzmrak
matevzmrak over 9 years ago

Hello forumers,

 

I am using RPi3 and I would like to use internet and receive calls at the same time.

 

I already tried that with USB modem HUAWEI E220 but there was no success. I also have HUAWEI E3531.

 

I just need internet connection to be running all the time and when I receive call I just get its number and cancel it without answering. When I get its number I need to check if it exists in database.

 

Do you know which USB modem / shield / modem should I use to perform this action?

 

----

 

I can read the number via AT commands, but I cannot use the internet connection at the same time because ports are busy.

 

import serial, re

command_channel = serial.Serial(
        port='/dev/ttyUSB0',
        baudrate=115200,
        parity=serial.PARITY_NONE,
        stopbits=serial.STOPBITS_ONE,
        bytesize=serial.EIGHTBITS
)

if(command_channel.isOpen() == False):
    command_channel.open()
else:
    print 'Port is already open'

#enable caller id
command_channel.write("AT+CLIP=1" + "\r\n")
# command_channel.close()

ser = serial.Serial(
        port='/dev/ttyUSB1',
        baudrate=9600,
        parity=serial.PARITY_NONE,
        stopbits=serial.STOPBITS_ONE,
        bytesize=serial.EIGHTBITS
)

if(ser.isOpen() == False):
    ser.open()
else:
    print 'Port is already open'

while 1:
        buffer = ser.read(ser.inWaiting()).strip()
        buffer = buffer.replace("\n","")
        
        if((str(buffer)).startswith('+CLIP')):  
            print(str(buffer)) # number


            if(command_channel.isOpen() == False):
                command_channel.open()
            else:
                print 'Port is already open'

            # cancel the call
            command_channel.write('AT+CVHU=0'+'\r\n')
            command_channel.write('ATH'+'\r\n')


            command_channel.close()

 

And I can connect to internet with VW dial using this config:

 

[Dialer defaults]
Phone = *99***1#
Username = username
Password = password
Stupid Mode = 1
Dial Command = ATDT

[Dialer hsdpa]
Modem = /dev/ttyUSB0
Baud = 460800
Init2 = ATZ
Init3 = ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0
ISDN = 0
Modem Type = Analog Modem

 

And the connection output:

 

pi@raspberrypi:~ $ sudo wvdial hsdpa
--> WvDial: Internet dialer version 1.61
--> Initializing modem.
--> Sending: ATZ
OK
--> Sending: ATZ
ATZ
OK
--> Sending: ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0
ATQ0 V1 E1 S0=0 &C1 &D2 +FCLASS=0
OK
--> Modem initialized.
--> Sending: ATDT*99***1#
--> Waiting for carrier.
ATDT*99***1#
CONNECT
--> Carrier detected.  Starting PPP immediately.
--> Starting pppd at Mon Feb  6 15:54:35 2017
--> Pid of pppd: 2206
--> Using interface ppp0
--> local  IP address 172.17.245.69
--> remote IP address 10.64.64.64
--> primary   DNS address 109.239.187.4
--> secondary DNS address 109.239.187.20

 

The problem is that I use ttyUSB0 to send AT command and ttyUSB1 to read the CLIP and RING messages, so I cannot use WVDIAL on these ports.

 

Should I buy a new modem or any other solution exists?

 

Thank you for your help image

 

BR, Matevz

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 9 years ago

    One modem connected to the RPi3 cannot service the internet and voice calls simultaneously with one account. The connection to the cell tower is limited.Now if you have two modem and two accounts that would be different.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 9 years ago

    One modem connected to the RPi3 cannot service the internet and voice calls simultaneously with one account. The connection to the cell tower is limited.Now if you have two modem and two accounts that would be different.