Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Camera and GPS not recognized
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 705 subscribers
  • Views 658 views
  • Users 0 members are here
  • raspberry_pi
Related

Raspberry Camera and GPS not recognized

jesusvaz
jesusvaz over 9 years ago

Raspberry,

 

I have a raspberry pi 3 model B. Mi goal is to take pictures and get the gps longitude and latitude. I got three cameras to test and a gps. All of them get connected using USB  ports.

I am using Python to get this data. The problem is that the devices get not recognized

And I get the following error for the camera:

 

raise SerialException("could not open port %s: %s" % (self._port, msg))se

SerialException: could not open port /dev/ttyACMO: [Errno 2] No such file or directory: '/dev/ttyACMO'

 

The gps throws a similar error.

 

I know the cameras and GPS are Raspberry compatibles but i think something changed

 

I have done a lot of research and it looks i have to do changes to the UART:

http://raspberrypi.stackexchange.com/questions/45570/how-do-i-make-serial-work-on-the-raspberry-pi3

 

But still i do not know if this is the correct path.

 

My Mac and Raspberry miss the  /dev/ttyACMO.

 

Thanks in advance.

 

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Jesus,

     

    Type lsusb  to see if the GPS unit gets detected when you plug it in.

    Then type ls /dev and see if anything gets added when the device is plugged in (compare it with the output of ls /dev when the device was not plugged in). It could be /dev/ACM0 but it may be something else.

    Also, your output text says ACMO but it never is ACMO. It could be ACM0 (you have character 'O' mixed with digit zero).

    If that is in the Python code or on the command line, it needs to be corrected to match what appears when the device is plugged in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi Jesus,

     

    Type lsusb  to see if the GPS unit gets detected when you plug it in.

    Then type ls /dev and see if anything gets added when the device is plugged in (compare it with the output of ls /dev when the device was not plugged in). It could be /dev/ACM0 but it may be something else.

    Also, your output text says ACMO but it never is ACMO. It could be ACM0 (you have character 'O' mixed with digit zero).

    If that is in the Python code or on the command line, it needs to be corrected to match what appears when the device is plugged in.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer