Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Is there onboard / built-in speakers or will I still need to connect my own?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 705 subscribers
  • Views 442 views
  • Users 0 members are here
  • raspberry_pi
  • raspeberry_pi_accessories
Related

Is there onboard / built-in speakers or will I still need to connect my own?

suth97
suth97 over 9 years ago

Want to hook this up to Raspberry Pi 3.

  • Sign in to reply
  • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago

    This is the second thread in which you've asked this.

    I guess that no one bothered to answer because it's kind of obvious from the spec;

     

    A quick Google and found the spec on E14 website and from it I extracted this:

     

    • For use with Raspberry Pi
    • Capable of rendering HD Audio, at 24-bit, 192kHz
    • 3.5mm 4-pole jack for a headset/boom mic combination for gaming or VoIP applications
    • Two DMIC microphones onboard for stereo recording
    • 3.5mm jack for Stereo Line Input for high quality audio recording or capture
    • 3.5 mm jack Stereo Line Output for connection to devices such as external stereo amplifiers or powered speakers
    • Stereo Digital input and output (SPDIF)

     

     

    So no speakers.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • marcelheijkoop
    0 marcelheijkoop over 9 years ago in reply to michaelkellett

    Derek, Michael,

     

    The Cirrus Logic Audio Card , is the only one compatible with a pi3, as for its 40 pins GPIO bus.

    The Cirrus Logic Audio Card , has its on board amp, capable of driving 2 speakers at about 3 watt per channel.

    However these pins are not soldered on from the factory, and must be done yourself.

    If you have the card and the skills, I advise you to do so and test it. The usecase scripts are provided.

     

    So quite obviously no on-board speakers on this card , but an on-board speakers out circuit is provided.

     

    I do not own a wolfson card, but they could be very similar, for the 1st generation raspberries of course.

     

    Regards,