Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Query regarding Touchscreen for RPi 3 running Debian Jessie
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 1 answer
  • Subscribers 710 subscribers
  • Views 1935 views
  • Users 0 members are here
  • debian jessie
  • touch screen
  • raspberry_pi
  • raspberry_pi_3
Related

Query regarding Touchscreen for RPi 3 running Debian Jessie

satyavrat
satyavrat over 9 years ago

I'm planning on buying a touchscreen display for my RPi 3, but I've read discussions where people claim that it doesn't work with Debian Jessie.

Can anyone please clarify this for me?

  • Sign in to reply
  • Cancel
Parents
  • dgoadby1
    0 dgoadby1 over 9 years ago

    Well, you don't say which type of touch screen you are thinking of buying. I use the type which has an HDMI screen and a USB touch screen interface. I upgraded from RPi2 to RPi3 and there were few problems other than the usual config file tweaks.

     

    I use the RPi in my products and that's the reason I use the HDMI/USB form as I am sure it will always work - even RPi4! Implementations that use the DSI port or SPI for the video will always have more of a dependency on the driver files being updated. The USB touch screen is also standard in Linux and only needs calibrating usually.

     

    If this is a one-off project then most of the LCD touch screens available should work on RPi3 and will say so in the documentation. Certainly the official screen does work as I have colleagues that use it.

     

    As most of my software is written in Python I use Kivy for the GUI. The nice thing about Kivy is I can develop my software on my main PC and it will run unaltered on the Rpi target. Yes, you can use Tkinter or QT, but Kivy is worth a look before you cut too much code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dgoadby1
    0 dgoadby1 over 9 years ago

    Well, you don't say which type of touch screen you are thinking of buying. I use the type which has an HDMI screen and a USB touch screen interface. I upgraded from RPi2 to RPi3 and there were few problems other than the usual config file tweaks.

     

    I use the RPi in my products and that's the reason I use the HDMI/USB form as I am sure it will always work - even RPi4! Implementations that use the DSI port or SPI for the video will always have more of a dependency on the driver files being updated. The USB touch screen is also standard in Linux and only needs calibrating usually.

     

    If this is a one-off project then most of the LCD touch screens available should work on RPi3 and will say so in the documentation. Certainly the official screen does work as I have colleagues that use it.

     

    As most of my software is written in Python I use Kivy for the GUI. The nice thing about Kivy is I can develop my software on my main PC and it will run unaltered on the Rpi target. Yes, you can use Tkinter or QT, but Kivy is worth a look before you cut too much code.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • uscdadnyc
    0 uscdadnyc over 9 years ago in reply to dgoadby1

    To DG. Nice post. You are spot-on w/ your comments concerning what are the Aim(s) of SW's project. Here, Form follows Function. A 2.5"er is more appropriate for him. DG (you) wrote>>...I use the HDMI/USB form as I am sure it will always work - even RPi4!...

    USCDADNYC Reply>> Yes, HDMI is more Universal than the SW's 2.5"er. But HDMI is Not Touch Screen. I got the best of both worlds. W/ my SmartiPi Touch Enclosure, I used a Dremel Tool to cut-away Access to the HDMI Port. Then used a Right-Angle HDMI-HDMI-Adapter. BTW RPi4? Do you know something, we don't. BTW2 I have on-order a Pi-TopCREED. for my next project. A Prototyping enclosure for possibly (a) RaspPiZeroW, (b) UP board (not UP^2 board), (c) RPi4(?) if form factor is not bigger than RPi3B. This Pi-TopCREED has a HDMI/eDP-to 14" LCD Display inside it.At least I think so. I will know better when I receive shipment.

    DG wrote>>...The USB touch screen is also standard in Linux...

    USCDADNYC Reply>> What USB Touch Screen? the official RPi 7" touch screen (element14.com, Stock # 49Y17120)?

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago in reply to dgoadby1

    Since yesterday post here, I have looked at Kivy. Very nice and open source too. Thanks for mentioning it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • COMPACT
    0 COMPACT over 9 years ago in reply to clem57

    Aha! It was you how opened my Tomato Source. image