Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum USB not working after wiping SD Card
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 12 replies
  • Answers 3 answers
  • Subscribers 710 subscribers
  • Views 2505 views
  • Users 0 members are here
  • keyboard
  • noobs
  • usb power
  • raspberry pi
Related

USB not working after wiping SD Card

iholman
iholman over 9 years ago

I've recently re-flashed my Pi, wiped the whole lot and put 'NOOBS_LITE_V2_4'. After plugging it back in, it powers up correctly, i get to the Noobs installation screen but the USB ports don't seem to work at all! So i cant install 'LibreELEC' because theres no power to to my keyboard.

 

I used to use my phone to control the Pi - but since wiping i cant do that either.

 

Anybody know why this would be happening, or if theres a way to tell if the ports are dead or just has the wrong software installed?

 

Any help is appreciated, cheers guys.

  • Sign in to reply
  • Cancel
  • rachaelp
    0 rachaelp over 9 years ago

    What Pi are you using? I think there was a change in the clocking to the IC which provides USB and Ethernet at some point and there were config changes made in the SD card image to support that for newer Pi versions. Somebody more familiar with the Pi (I've not used my old Pi model B for quite a while!) will be able to confirm but I suspect it's something in the config which is not enabling the clock to that IC, hence the USB doesn't work.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 9 years ago

    Go to a powered hub which can be had for a few $$$.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 9 years ago in reply to clem57

    Like the advertisement for M&M Candies' Mounds & Almond-Joy. "Sometimes you feel like a Nut. Sometimes you Don't". Here sometimes you need a Powered Hub. Sometimes you Don't. I made myself a cable that turns an Un-powered Hub into a Powered Hub. Of course it also turns the Hub into USB 2.0, b/c I only used Red, Blk, Wht, Grn Leads. I may open-up my Bidul USB Hub 3.0 w/ Ethernet Adapter, and make changes in there. Then it maintains it's USB 3.0 characteristics

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iholman
    0 iholman over 9 years ago in reply to rachaelp

    It's the raspberry pi 2 (B) - If it's something in the config, how do i go about changing that? I was hoping by formatting and putting Noobs back on there it'd work like i had it before.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • iholman
    0 iholman over 9 years ago in reply to clem57

    I thought powered hubs work by connecting into the USB (And mains) - If the USB on the pi don't work, i wont get connectivity to it right?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jlangbridge
    0 jlangbridge over 9 years ago in reply to iholman

    That is indeed how they work. A USB port can supply a small amount of current, and depending on the device that has the USB port, this value changes. The Raspberry Pi can't deliver much (actually, there were stories of simple USB keys that would make the Pi reboot when inserted due to power drain). If a device pulls too much power, it is simply deactivated, which might be the case here. If your keyboard is pulling too much power, then the RPi shuts it down, and nothing works. By plugging in a powered USB hub, the Pi doesn't actually need to supply any energy, so everything connected to the hub, and powered by the hub, should be visible.

     

    I'm not too sure how to debug your situation. I have a wireless keyboard/mouse combo that I use for my RPis, and I've never had a problem. I have had the USB key problem (which is a long story), so I know from experience that RPis can be a bit tricky, but a standard keyboard (not a flashy model with RGB LEDs) should work... Do you have a multimeter, or some way to test if the USB port is powered?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • iholman
    0 iholman over 9 years ago in reply to jlangbridge

    Would this be suitable?

     

    https://thepihut.com/products/7-port-usb-hub-for-the-raspberry-pi?utm_medium=cpc&utm_source=googlepla&variant=763067941&…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rew
    0 rew over 9 years ago in reply to jlangbridge

    Small addition: The pi 1 has a sort-of-fuse in the USB that shuts off stuff when it draws too much power. IIRC this worked shitty and was removed quite quickly. So it might have been: "early raspberry pi 1 boards"....

     

    The latest pi 3 has a dedicated chip arranging power for the USB ports. It powers up the USB port only after booting, and the chip will monitor the port for too much power and shut it down if that happens. I'm not entirely sure what the pi2 has.

     

    (I have a many-port powered hub (15A power supply... plenty!), which I use to distribute power to several pi's on my desk. One of them is the "master" of all the other devices in that hub. So it has one cable for power, and the other from the USB port on the pi to the input port on the hub.... So when I unplug the pi's power because it needs to be powered down... it stays up. The hub will back-feed the pi. But when I unplug the input to the hub, the pi shuts down and doesn't come back up when I reconnect the USB-output-to-hub-input cable. It needs the power cable for a few seconds to enable the downstream USB ports....)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jlangbridge
    0 jlangbridge over 9 years ago in reply to iholman

    Looks good! Something like that should work. However, the title of your post still worries me... USB not working after SD wipe, that shouldn't change anything for the USB ports; if they worked before, they should still work now. I haven't looked, but I believe that NOOBS works for all Pis, so there shouldn't be a driver difference.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago in reply to iholman

    Ive got libreELEC on a raspberry Pi 2 B and theres no problem with the USB, could it be the NOOBS installer/config causing the problem? Try going to the libreELEC website and flash the direct image from there, that way it cuts out the need to use the NOOBS installer.

     

    https://libreelec.tv/downloads/

     

    Scroll halfway down the page and there a compressed image for raspberry pi's, You'll need to be able to uncompress the .gz file and then flash the resulting .img file to the sdcard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>