Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help me feed a Power Hungry RPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 1805 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Help me feed a Power Hungry RPi

dzed
dzed over 9 years ago

I've just completed building a kit  with a 7" touch screen and  RPi 3B.

 

The  tutorial I found  presented   3 options for  powering the  kit..

 

A.  Cable from the USB power out on the display board to the Micro USB power in.    Id rather NOT make holes in the case supplied to enable  this.

 

B . GPIO power bridge to the display board via  jumpers  ( The option I selected)

 

C. 2 Micro usb power connectors,  1 to the display board and  1 to the  RPi...  

 

After assembly and some use I've noticed the  "lightning flash" on the upper right,  which I understand indicates a low power condition.

I'm using the "standard" 5V/ 2.5A RPi 3B wall plug..   and the unit  "works"   with power applied to either of the inputs...

 

My questions.... 

    

     What am I really  risking  running the unit  in an underpowered condition???   Is it just throttling the  CPU back?

 

     Is it safe to apply power to both USB inputs  with the GPIO powers jumpers in place?

 

     Are there any "known hacks" to reduce the power consumption of the display to minimize the impact?

  • Sign in to reply
  • Cancel
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi,

     

    That's not normal if the official Pi 7" touchscreen and official power supply (with permanently wired cable with micro USB connector) is used.

    Depending on the work load, the Pi 3 can consume a lot of power (up to 1.4A at 5V), but you'd soon know if you were, because the CPU would get extremely hot, too hot to touch.

    If you wish to test with a supply powering the display separately, then the power jumpers connected to the 40-way connector should be disconnected.

    In the underpowered condition there could be a risk of corruption or any USB attached devices not operating correctly.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 9 years ago

    Hi,

     

    That's not normal if the official Pi 7" touchscreen and official power supply (with permanently wired cable with micro USB connector) is used.

    Depending on the work load, the Pi 3 can consume a lot of power (up to 1.4A at 5V), but you'd soon know if you were, because the CPU would get extremely hot, too hot to touch.

    If you wish to test with a supply powering the display separately, then the power jumpers connected to the 40-way connector should be disconnected.

    In the underpowered condition there could be a risk of corruption or any USB attached devices not operating correctly.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • dzed
    0 dzed over 9 years ago in reply to shabaz

    Thanks for the feedback (everyone)...

     

    I've reflashed the  SDC with a copy of Ubuntu Mate (16.10)  and used the display slider to reduce the screen brightness to ~= 30%.

     

    I still get the power indicator briefly at boot time,  but only  very  occasionally  after that.    I've run the RPi the better part of a day, and the  case ventilation seems to be adequate to keep the  CPU/GPU temperature at reasonable ( Warm to the touch) levels, indicating it is probably the display.    I'd hoped to minimize the number of cables external to the case, but changing the battery power unit to one with 2USB outlets is a viable design change..   I will make sure to remove the GPIO power jumpers before testing that out... 

     

    It's a little concerning that the panel seems to be  "abnormally thirsty", but I'm still impressed/pleased with the overall performance.