Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Help me feed a Power Hungry RPi
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 707 subscribers
  • Views 1805 views
  • Users 0 members are here
  • raspberry_pi_space
Related

Help me feed a Power Hungry RPi

dzed
dzed over 9 years ago

I've just completed building a kit  with a 7" touch screen and  RPi 3B.

 

The  tutorial I found  presented   3 options for  powering the  kit..

 

A.  Cable from the USB power out on the display board to the Micro USB power in.    Id rather NOT make holes in the case supplied to enable  this.

 

B . GPIO power bridge to the display board via  jumpers  ( The option I selected)

 

C. 2 Micro usb power connectors,  1 to the display board and  1 to the  RPi...  

 

After assembly and some use I've noticed the  "lightning flash" on the upper right,  which I understand indicates a low power condition.

I'm using the "standard" 5V/ 2.5A RPi 3B wall plug..   and the unit  "works"   with power applied to either of the inputs...

 

My questions.... 

    

     What am I really  risking  running the unit  in an underpowered condition???   Is it just throttling the  CPU back?

 

     Is it safe to apply power to both USB inputs  with the GPIO powers jumpers in place?

 

     Are there any "known hacks" to reduce the power consumption of the display to minimize the impact?

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    I agree with shabaz and with the official power unit something sounds not normal. If this can be helpful I have used continuously for some days a PI3b + LCD 7 inches, using ther ethernet cable connected to a computer. The CPU was almost stressed as I was testing and developing, the LCD never was in standby mode and in addition I was using through the local LAN the PI from the Display itself (testing graphic UI), a VNC connection and the ssh shell so as a matter of fact there was three users connected at the same time to the Pi. Then the PI /home/pi folder was shared with the PC and remotely mounted. With this scenario I had no problem in powering the system and I have also tried to power the system with a battery unit supply of 2.4 A (7600 mA/h) and it worked perfectly in test for about 6 hours.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • uscdadnyc
    0 uscdadnyc over 9 years ago in reply to balearicdynamics

    EM wrote>>...[I] power[ed] the system [RPi-TFT screen] with a battery unit supply of 2.4 A (7600 mA/h)...

    USCDADNYC Question>> Is there a (mathematical) relationship between 2.4A and 7600 mA/h?

    USCDADNYC (NY NY USA)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • uscdadnyc
    0 uscdadnyc over 9 years ago in reply to balearicdynamics

    EM wrote>>...[I] power[ed] the system [RPi-TFT screen] with a battery unit supply of 2.4 A (7600 mA/h)...

    USCDADNYC Question>> Is there a (mathematical) relationship between 2.4A and 7600 mA/h?

    USCDADNYC (NY NY USA)