Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 B - Illuminated Power Switch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 706 subscribers
  • Views 709 views
  • Users 0 members are here
  • gpio
  • raspberry_pi
  • button
  • power switch
Related

Raspberry Pi 2 B - Illuminated Power Switch

j666gak
j666gak over 9 years ago

Hello,

 

I have been searching across the forum for articles relation to adding a power button, however all of the posts either refer to using GPIO pins 5 & 6 which I am already using for the offical 7" touchscreen.

 

  • Can either momentary or latching switch be used?
  • Which GPIO could be used instead on pins 5/6? or does it have to be 5v and ground
  • On the switch would you normally NO (Normally Open) or NC (Normally Closed) terminal?

 

Thanks for your help in advance.

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Guy,

    O think that the best solution to manafe a power button is just using pins 5 and 6

    There more power options instead to power both the PI and the touch together. Tje most affordable is to power the lcd micro USB and connect the PI from the second ISB B on the display controller board to the micro USB. Then you have both the devices connected with a single power line. Then with your power unit connected to the pin 5 and 6 the entire system will work as expected.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 9 years ago

    Hello Guy,

    O think that the best solution to manafe a power button is just using pins 5 and 6

    There more power options instead to power both the PI and the touch together. Tje most affordable is to power the lcd micro USB and connect the PI from the second ISB B on the display controller board to the micro USB. Then you have both the devices connected with a single power line. Then with your power unit connected to the pin 5 and 6 the entire system will work as expected.

     

    Enrico