Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum Raspberry Pi 2 B - Illuminated Power Switch
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 706 subscribers
  • Views 706 views
  • Users 0 members are here
  • gpio
  • raspberry_pi
  • button
  • power switch
Related

Raspberry Pi 2 B - Illuminated Power Switch

j666gak
j666gak over 9 years ago

Hello,

 

I have been searching across the forum for articles relation to adding a power button, however all of the posts either refer to using GPIO pins 5 & 6 which I am already using for the offical 7" touchscreen.

 

  • Can either momentary or latching switch be used?
  • Which GPIO could be used instead on pins 5/6? or does it have to be 5v and ground
  • On the switch would you normally NO (Normally Open) or NC (Normally Closed) terminal?

 

Thanks for your help in advance.

  • Sign in to reply
  • Cancel
Parents
  • vandia
    0 vandia over 9 years ago

    I've never used the Pi display you're referring to, but I presume you can change the GPIO you're charging it with, as Enrico said.

     

    That option aside, you also have the option to have a switch to the system's power input instead:
    -There is a Micro USB cable with power switch you can buy
    -You can splice to add a switch to the Micro USB wire.

     

    I've not heard of using a switch on the GPIOs to control the power, and while some object to unplugging power when something's on, it's all I do with the Pi. In fact, I personally would see more risk to trying to short the system with a switch on the GPIOs, than using a switch to control the power.

     

    I know you're likely wanting to "do a thing" with the Pi, but sometimes, hardware is a better method than software.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • vandia
    0 vandia over 9 years ago

    I've never used the Pi display you're referring to, but I presume you can change the GPIO you're charging it with, as Enrico said.

     

    That option aside, you also have the option to have a switch to the system's power input instead:
    -There is a Micro USB cable with power switch you can buy
    -You can splice to add a switch to the Micro USB wire.

     

    I've not heard of using a switch on the GPIOs to control the power, and while some object to unplugging power when something's on, it's all I do with the Pi. In fact, I personally would see more risk to trying to short the system with a switch on the GPIOs, than using a switch to control the power.

     

    I know you're likely wanting to "do a thing" with the Pi, but sometimes, hardware is a better method than software.