Raspberry Pi
  • Products
  • More
Raspberry Pi
Raspberry Pi Forum boot from ssd in pi desktop
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Raspberry Pi to participate - click to join for free!
Featured Articles
Announcing Pi
Technical Specifications
Raspberry Pi FAQs
Win a Pi
Raspberry Pi Wishlist
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 73 replies
  • Answers 11 answers
  • Subscribers 715 subscribers
  • Views 13037 views
  • Users 0 members are here
  • raspberry_pi_space
Related

boot from ssd in pi desktop

gdenicolas
gdenicolas over 9 years ago

I couldnt find the file pidesktop.deb. The webpage is really complicated.

  • Sign in to reply
  • Cancel
Parents
  • cstanton
    0 cstanton over 9 years ago

    Hi gdenicolas ,

     

    You don't need the debian file to boot from the SSD. In the user manual is a step by step guide and explanation on how to set this up:

    Pi Desktop User Manual_EN_Rev3.2-FINAL.pdf

     

    I've asked internally about the debian file, and I've read through the manual where there's some typing errors that need to be fixed (eg. capitalization of linux commands).

     

    Feel free to ask me any questions on this as I've been working with this add-on board (and have one sat on my desk).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    My concern not loading the pidesktop.deb is that you lose out on :

     

    ppp-hdclone (What it does probably can be done just by dd'ing the image to the mSata)

     

    ppp-boot (This actually changes the /boot/cmdline.txt to change the root, which isn't mentioned. I had previously set the usb variable, but AFTER I put it all together so can't get the card out to test if it isn't needed)

     

    embest.service/embest-shutdown.service/rtc.py/sync-hwclock - Seem like they make sure the HWClock is up to date, not mentioned in the manual.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    The SDCard isn't needed when booting from USB after the bit is set. The Pi prioritises booting from SDCard if it is inserted as well as the USB device.

     

    If you have only a USB bootable device inserted, and the SDCard removed, you don't have to change the location in /boot/cmdline.txt. It's probably best to set the bit before putting the Pi inside the enclosure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    The SDCard isn't needed when booting from USB after the bit is set. The Pi prioritises booting from SDCard if it is inserted as well as the USB device.

     

    If you have only a USB bootable device inserted, and the SDCard removed, you don't have to change the location in /boot/cmdline.txt. It's probably best to set the bit before putting the Pi inside the enclosure.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    None of that was in any doco I received. image I actually got it all running by trial/error. I used a small SD card so don't care about its loss. But nice to have the deb for the extra RTC stuff.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    tuctboh

    You're right that it doesn't say which device it prioritises, though it does say on page 15 that the SD Card is no longer needed. Do you feel it should be explicitly stated to remove the SD Card ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Yes, do think it would be useful. I think even more useful is telling you to install the "Type A to micro USB" *BEFORE* you put the lid on. I found I needed to pry the lid off (Whoever designed it meant for it NEVER to come off. image ) and press/lift the hat ever so slightly to get it to align JUST right. The 2nd time I put it together when I was testing things I ended up doing it outside the case so I could take out/put in the SD card... So it really is out of the case. Adds a nice blue glow to my work room

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    So I shutdown the Pi, pulled the SD card, turned it on, waited 15 seconds... Nothing. Put the card, started up, checked that my /boot and / were running off the mSata (I changed the /boot/cmdline.txt on the SD), and ran "vcgencmd otp_dump | grep 17:" and got the right response of 0x3020000a. Shut down, pulled the card, tried again, nothing.

     

    The mSata was loaded by booting off SD, dd of the Raspbian Jessie to it, then I did by hand the expand of partition 2 (Delete, extend, resize2fs).

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    If you've dd'd the default Raspbian Jessie image from raspberrypi.org to the SSD you don't need to change the contents of cmdline.txt on the SSD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    I didn't. It was on the SD I made the changes. But still the issue that despite having the 0x3020000a set, it isn't booting from SSD.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    Tuc . wrote:

     

    Hi,

     

    I didn't. It was on the SD I made the changes. But still the issue that despite having the 0x3020000a set, it isn't booting from SSD.

     

    Tuc

    When I initially imaged the SSD it didn't boot either, and that was because of the software I used to write the image to the SSD didn't do it properly.

     

    What software/commands have you used to write the image to the SSD and under which operating system?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Raspbian Pixel, fresh install to the SD.

     

    unzip -p|dd bs=1m of=/dev/sda

     

    I think thats it. Might be uppercase M, I get confused, some platforms take it, others don't. I didn't have space on the 8G card in it, so I had to stream the contents of the download and pipe into dd.

     

    Tuc

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 9 years ago in reply to tuctboh

    I would suggest trying either the hard drive clone script that's included with the debian package to replicate your SDCard raspbian install, or try imaging the SSD by connecting it to another computer (this is outlined in the manual).

     

    Have you tried wiping the SSD and partitioning it via other ways (not imaging it) to see if it's compatible and working in with the Pi HAT add-on? There could be something funny going on there, too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • tuctboh
    0 tuctboh over 9 years ago in reply to cstanton

    Hi,

     

    Unfortunately, I can't. I don't own anything else that can take the mSata card (https://smile.amazon.com/gp/product/B00TGIVRYU ). The Pi-Desktop is the only thing.

     

    Tuc